Other Parts Discussed in Thread: CC3220SF, UNIFLASH, TIDC-01005, CC3220S
Hello everyone,
I have been working on CC3220SF for a whiile now using the cc3220sf launhpad.
I have dumped the code using uniflash initially to get into development mode later i have loaded the example applications from ti explorer Code composer studio(CCS Version: 9.2.0.00013 ) and everything is working fine.
Now i am building my application on the reference design (TI Designs: TIDC-01005 Battery-Powered, Smart-Lock Reference Design With Cloud Connectivity Using SimpleLink™ Wi-Fi) which is built on CC3220S.
i have downloaded the code and imported to my workspace and I have changed the device to CC3220SF from CC3220S in properties and have added the required .cmd file(CC3220SF_LAUNCHXL_TIRTOS.cmd) .
and have built it successfully after adding the required SDK and other plugins without errors.
ISSUE:
Now the issue is i am getting the following error when try to debug the code from CCS .
I can see the firmware loading but when i press the run(play) button in CCS i observe the following error.
Cortex_M4_0: JTAG Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.3.0.00003)
Cortex_M4_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
What might be issue?
Note: All the other example firmwares are working fine
Regards,
Sanath Rai