Part Number: BOOSTXL-CC3135
Other Parts Discussed in Thread: CC3135, UNIFLASH, CC3100SDK, CC3100, CC3120
Hello. I am trying to use CC3135 using STM32f103 (Nucleo board) by porting SimpleLink CC3100SDK 1.3.0. I have uploaded the service pack 4.1.0.28_3.1.0.5_3.1.0.17 (most recent version) through Uniflash.
During porting the SDK, I replaced the SPI related function (spi_open, read, write, close) based on the pre-defined function like MX_SPI_Init(), MX_GPIO_Init() through CUBEmx. Furthermore, I have added needed event handlers and functions to deal with the interrupt signal from the IRQ pin from the CC3135.
Problems are the return value of sl_Start is always 1 (ROLE_UNKNOWN) and the program get stuck at the 'SL_DRV_SYNC_OBJ_WAIT_TIMEOUT' when I call sl_Stop(). In the case of sl_Stop, if I call the sl_Stop(0), then it does not get stuck.
The wired point is that, if I set the AP mode to the CC3135 using sl_WlanSetModeI(ROLE_AP), zero is returned and I can search the AP in my cell phone or laptop. This AP can be appeared and disappeared on my cell phone when I call sl_start and sl_Stop(0), repeatedly.
Also, if I called the sl_NetCFgGet to get the MAC address of the CC3135, it returns 0 which shows there is no problem during the command. However, the returned MAC address (macAddressVal[]) were 0x3, 0x34, 0x0, 0x6, 0x0, 0x0 which cannot be believed as the MAC address.
I doubt that my MCU (STM32F103) may not be able to read proper data through SPI, is it correct?
I wonder what I can solve these problems.
Source code: main.c
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2019 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "simplelink.h"
#include "sl_common.h"
#include "user.h"
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
SPI_HandleTypeDef hspi2;
TIM_HandleTypeDef htim1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
#define ASSERT_CS() (HAL_GPIO_WritePin(SPI2_CS_GPIO_Port, SPI2_CS_Pin, GPIO_PIN_RESET))
#define DEASSERT_CS() (HAL_GPIO_WritePin(SPI2_CS_GPIO_Port, SPI2_CS_Pin, GPIO_PIN_SET))
#define SPI_TIMEOUT_MAX 0x1000
#define SCAN_TABLE_SIZE 20
#define SCAN_INTERVAL 10
P_EVENT_HANDLER pIrqEventHandler = 0;
Sl_WlanNetworkEntry_t netEntries[SCAN_TABLE_SIZE];
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_SPI2_Init(void);
static void MX_TIM1_Init(void);
/* USER CODE BEGIN PFP */
static _i32 initializeAppVariables();
static _i32 establishConnectionWithAP();
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
_u32 g_Status = 0;
_u32 g_PingPacketsRecv = 0;
_u32 g_GatewayIP = 0;
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_SPI2_Init();
MX_TIM1_Init();
/* USER CODE BEGIN 2 */
int retVal = 0;
retVal = sl_Start(0, 0, 0);
retVal = sl_WlanSetMode(ROLE_AP);
retVal = sl_Stop(0);
retVal = sl_Start(0, 0, 0);
_u8 macAddressVal[SL_MAC_ADDR_LEN];
_u8 macAddressLen = SL_MAC_ADDR_LEN;
sl_NetCfgGet(SL_MAC_ADDRESS_GET,NULL,&macAddressLen,(_u8 *)macAddressVal);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI_DIV2;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL16;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief SPI2 Initialization Function
* @param None
* @retval None
*/
static void MX_SPI2_Init(void)
{
/* USER CODE BEGIN SPI2_Init 0 */
/* USER CODE END SPI2_Init 0 */
/* USER CODE BEGIN SPI2_Init 1 */
/* USER CODE END SPI2_Init 1 */
/* SPI2 parameter configuration*/
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI2_Init 2 */
/* USER CODE END SPI2_Init 2 */
}
/**
* @brief TIM1 Initialization Function
* @param None
* @retval None
*/
static void MX_TIM1_Init(void)
{
/* USER CODE BEGIN TIM1_Init 0 */
/* USER CODE END TIM1_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_SlaveConfigTypeDef sSlaveConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM1_Init 1 */
/* USER CODE END TIM1_Init 1 */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 64;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 0;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_DISABLE;
sSlaveConfig.InputTrigger = TIM_TS_ITR0;
if (HAL_TIM_SlaveConfigSynchro(&htim1, &sSlaveConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM1_Init 2 */
/* USER CODE END TIM1_Init 2 */
}
/**
* @brief USART2 Initialization Function
* @param None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOB, CC_nHIB_Pin|SPI2_CS_Pin, GPIO_PIN_SET);
/*Configure GPIO pin : B1_Pin */
GPIO_InitStruct.Pin = B1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : LD2_Pin */
GPIO_InitStruct.Pin = LD2_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(LD2_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : CC_EXTI_Pin */
GPIO_InitStruct.Pin = CC_EXTI_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(CC_EXTI_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pins : CC_nHIB_Pin SPI2_CS_Pin */
GPIO_InitStruct.Pin = CC_nHIB_Pin|SPI2_CS_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI2_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(EXTI2_IRQn);
HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
}
/* USER CODE BEGIN 4 */
void SimpleLinkGeneralEventHandler(SlDeviceEvent_t *pDevEvent)
{
/*
* Most of the general errors are not FATAL are are to be handled
* appropriately by the application
*/
}
void SimpleLinkHttpServerCallback(SlHttpServerEvent_t *pHttpEvent,
SlHttpServerResponse_t *pHttpResponse)
{
/*
* This application doesn't work with HTTP server - Hence these
* events are not handled here
*/
}
void SimpleLinkSockEventHandler(SlSockEvent_t *pSock)
{
/*
* This application doesn't work w/ socket - Hence not handling these events
*/
}
void SimpleLinkNetAppEventHandler(SlNetAppEvent_t *pNetAppEvent)
{
if(pNetAppEvent == NULL)
{
return;
}
switch(pNetAppEvent->Event)
{
case SL_NETAPP_IPV4_IPACQUIRED_EVENT:
{
SlIpV4AcquiredAsync_t *pEventData = NULL;
SET_STATUS_BIT(g_Status, STATUS_BIT_IP_ACQUIRED);
pEventData = &pNetAppEvent->EventData.ipAcquiredV4;
g_GatewayIP = pEventData->gateway;
}
break;
default:
{
}
break;
}
}
void SimpleLinkWlanEventHandler(SlWlanEvent_t *pWlanEvent)
{
if(pWlanEvent == NULL)
{
return;
}
switch(pWlanEvent->Event)
{
case SL_WLAN_CONNECT_EVENT:
{
SET_STATUS_BIT(g_Status, STATUS_BIT_CONNECTION);
/*
* Information about the connected AP (like name, MAC etc) will be
* available in 'slWlanConnectAsyncResponse_t' - Applications
* can use it if required
*
* slWlanConnectAsyncResponse_t *pEventData = NULL;
* pEventData = &pWlanEvent->EventData.STAandP2PModeWlanConnected;
*
*/
}
break;
case SL_WLAN_DISCONNECT_EVENT:
{
slWlanConnectAsyncResponse_t* pEventData = NULL;
CLR_STATUS_BIT(g_Status, STATUS_BIT_CONNECTION);
CLR_STATUS_BIT(g_Status, STATUS_BIT_IP_ACQUIRED);
pEventData = &pWlanEvent->EventData.STAandP2PModeDisconnected;
/* If the user has initiated 'Disconnect' request, 'reason_code' is SL_USER_INITIATED_DISCONNECTION */
if(SL_WLAN_DISCONNECT_USER_INITIATED_DISCONNECTION == pEventData->reason_code)
{
}
else
{
}
}
break;
default:
{
}
break;
}
}
Fd_t spi_Open(char *ifName, unsigned long flags)
{
MX_SPI2_Init();
/* Initialize and disable the nHIB line */
CC3100_nHIB_init();
CC3100_disable();
Delay(50);
return 0;
}
int spi_Write (Fd_t fd, unsigned char *pBuff, int len)
{
ASSERT_CS();
HAL_SPI_Transmit(&hspi2, pBuff, len, SPI_TIMEOUT_MAX);
DEASSERT_CS();
return len;
}
int spi_Read(Fd_t fd, unsigned char *pBuff, int len)
{
ASSERT_CS();
HAL_SPI_Receive(&hspi2, pBuff, len, SPI_TIMEOUT_MAX);
DEASSERT_CS();
return len;
}
int spi_Close(Fd_t fd)
{
/* Disable Interrupt in GPIOA module... */
// CC3100_InterruptDisable();
HAL_Delay(100);
/* Deinitialize SPI */
HAL_SPI_DeInit(&hspi2);
HAL_Delay(100);
return 0;
}
void CC3100_nHIB_init()
{
MX_GPIO_Init();
}
void CC3100_disable()
{
HAL_GPIO_WritePin(CC_nHIB_GPIO_Port, CC_nHIB_Pin, 0);
}
void Delay(unsigned long delay)
{
HAL_Delay(delay);
}
int registerInterruptHandler(P_EVENT_HANDLER InterruptHdl , void* pValue)
{
pIrqEventHandler = InterruptHdl;
return 0;
}
void CC3100_enable()
{
HAL_GPIO_WritePin(CC_nHIB_GPIO_Port, CC_nHIB_Pin, 1);
}
unsigned long timer_GetCurrentTimestamp()
{
unsigned long timer_value = 0;
//Verify timer has been started by checking that the control register was set
if((TIM_CR1_CEN) != (((&htim1)->Instance->CR1) & (TIM_CR1_CEN)))
{
MX_TIM1_Init();
}
timer_value = __HAL_TIM_GET_COUNTER(&htim1);
return timer_value;
}
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
/* Prevent unused argument(s) compilation warning */
UNUSED(GPIO_Pin);
/* NOTE: This function Should not be modified, when the callback is needed,
the HAL_GPIO_EXTI_Callback could be implemented in the user file
*/
if((GPIO_Pin == CC_EXTI_Pin) &&
(NULL != pIrqEventHandler) )
{
pIrqEventHandler(0);
}
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */