Other Parts Discussed in Thread: TIDC-01005, , CC3220S, UNIFLASH, ENERGIA
Hello,
I am working on CC3220SF launchpad module.Working on wifi doorlock refer tidc-01005.which was designed for cc3220s but i have changed it to cc3220sf. which is working on SWD programming SOP setting is 001 on launchpad board.
1. I need to flash the code into cc3220sf that is on power reset the code should boot from flash which is not happening now its running on SRAM .i need to debug every time when the power reset occurs code dosen't boot.
what is the way to flash it like for production mode.
2. Right now i'm debugging and dumping my code via Code composer studio and i'm not not able to dump the .bin file of my project via uniflash (version 5.1.0)
My bin file is showing as 496Mb ...i dont know why its that big? but i can debug using CCS
i dont know the cause when i try to add the file in uniflash
the bin file(496Mb) using Uniflash as it is throwing the Error
Error:MCU Image file exceeds the maximum size for this device
i will attach the map file here
3. i have also tried dumping the .bin file via uniflash session using CC3220SF_SWD.ccxml file. getting below error