Other Parts Discussed in Thread: CC3100SDK, CC3120, , CC3100
On a custom hardware board the CC3120MOD is connected to a LPC54114 MCU by the 4-wire uart topology.
I started porting the TI wifi driver from the CC3100SDK_1.3.0 with the use of freeRTOS.
I modified the user.h as follows
#define sl_IfOpen uart_Open
#define sl_IfClose uart_Close
#define sl_IfRead uart_Read
#define sl_IfRegIntHdlr(InterruptHdl , pValue) //nothing
#define sl_IfMaskIntHdlr() //nothing
#define sl_IfUnMaskIntHdlr() //nothing
When I start with "sl_Start(0, 0, 0);"
The library is waiting in the sl_start routine at _SlDrvSyncObjWaitTimeout(..) function, I assume because of the missing host_IRQ connection.
Is this assumtion right?
Is there any instruction how to port the library in the 4-wire uart topology?