Hi,
While trying to setup a mesh network with a set of BeagleBone Green Wireless devices (that have the WL1835MOD chip), running the latest Debian 10 (buster) distro (with Linux kernel 4.19.94-ti-r42), I've hit a situation were I can connect the BeagleBones in mesh mode, but only without authentication set.
Looking at a previous post (Linux/WL1837MOD: 802.11s MESH + SAE), I've found the info that SAE only works with a modified wpa_supplicant from TI, so I've compiled it, following the instructions on the post, but still without success on the connectivity between the boards.
Is there any other thing that needs to be addressed to make mesh + SAE to work with BeagleBone Green Wireless devices running Debian 10?
Are TI not planning to push upstream the changes required to operate wl18xx devices in an authenticated (SAE) mesh?
Best regards,
José Gonçalves