Other Parts Discussed in Thread: UNIFLASH, , CC3235SF, CC3100, CC3200
Hi folks,
I am unable to load ImageCreator and tried both UniFlash 5 and the recently released v6.0.0.
When I select LAUNCHXL-CC3235SF from UniFlash, I get a spinning icon next to "Start Image Creator" as depicted in the attached pic.
If I attempt to start ImageCreator from the CLI, I get:
<uni flash root dir>/simplelink/imagecreator/bin/SLImageCreator Traceback (most recent call last): File "SLImageCreator.py", line 33, in <module> File "/private/var/folders/79/10c7185s6cn_8zc1hsk5rcdw0000gn/T/pip-install-Um7Hyj/pyinstaller/PyInstaller/loader/pyimod03_importers.py", line 396, in load_module File "logging/__init__.py", line 26, in <module> File "/private/var/folders/79/10c7185s6cn_8zc1hsk5rcdw0000gn/T/pip-install-Um7Hyj/pyinstaller/PyInstaller/loader/pyimod03_importers.py", line 396, in load_module File "weakref.py", line 14, in <module> from _weakref import ( ImportError: cannot import name _remove_dead_weakref [78672] Failed to execute script SLImageCreator
I am running this on MacOS.
What am I doing wrong?