Hi,
1. TI Wireless Tools on ti.com runs on the Windows operating system. Are there any wireless tools for the Linux operating system?
That is, how to search the nearby network on the Linux system, set the AP name and password according to different encryption methods, dynamically or statically assign ip methods, connect existing connections / disconnect wifi and other application operations through what application software ?
2. Before these applications can be used, what configuration operations do we need to perform on the kernel to support the wifi function of the sdio interface and the Bluetooth function of the uart interface? No relevant documentation was found. Does it only need to configure the kernel to drive the wifi and Bluetooth functions of this chip? Do I need other drivers?
Thanks
BRs
Elsa Duan