Other Parts Discussed in Thread: CC3120
Hi,
Can anyone help why I am getting this kind of response time variation or sometime timeout on ping command as I am using latest service pack and host driver,
This behavior observed in both AP and station mode but sometimes it work fine why?
==============================================
CHIP: 0x31000000
MAC: 2.0.0.0
PHY: 2.2.0.7
NWP: 3.15.0.1
ROM: 0
HOST: 3.0.1.41
MAC address: c8:df:84:4f:ba:f9
==============================================
Pinging 192.168.43.237 with 32 bytes of data:
Reply from 192.168.43.237: bytes=32 time=9ms TTL=128
Reply from 192.168.43.237: bytes=32 time=102ms TTL=128
Reply from 192.168.43.237: bytes=32 time=37ms TTL=128
Reply from 192.168.43.237: bytes=32 time=32ms TTL=128
Reply from 192.168.43.237: bytes=32 time=138ms TTL=128
Reply from 192.168.43.237: bytes=32 time=144ms TTL=128
Reply from 192.168.43.237: bytes=32 time=162ms TTL=128
Reply from 192.168.43.237: bytes=32 time=7ms TTL=128
Reply from 192.168.43.237: bytes=32 time=3ms TTL=128
Reply from 192.168.43.237: bytes=32 time=30ms TTL=128
Reply from 192.168.43.237: bytes=32 time=4ms TTL=128
Reply from 192.168.43.237: bytes=32 time=7ms TTL=128
Reply from 192.168.43.237: bytes=32 time=152ms TTL=128
Reply from 192.168.43.237: bytes=32 time=8ms TTL=128
Reply from 192.168.43.237: bytes=32 time=3ms TTL=128
Reply from 192.168.43.237: bytes=32 time=35ms TTL=128
Reply from 192.168.43.237: bytes=32 time=9ms TTL=128
Reply from 192.168.43.237: bytes=32 time=7ms TTL=128
Reply from 192.168.43.237: bytes=32 time=113ms TTL=128
Reply from 192.168.43.237: bytes=32 time=130ms TTL=128
Reply from 192.168.43.237: bytes=32 time=8ms TTL=128
Reply from 192.168.43.237: bytes=32 time=32ms TTL=128
Reply from 192.168.43.237: bytes=32 time=76ms TTL=128
Reply from 192.168.43.237: bytes=32 time=6ms TTL=128
Reply from 192.168.43.237: bytes=32 time=108ms TTL=128
Reply from 192.168.43.237: bytes=32 time=9ms TTL=128
Reply from 192.168.43.237: bytes=32 time=31ms TTL=128
Reply from 192.168.43.237: bytes=32 time=31ms TTL=128
Reply from 192.168.43.237: bytes=32 time=54ms TTL=128
Reply from 192.168.43.237: bytes=32 time=89ms TTL=128
Reply from 192.168.43.237: bytes=32 time=3ms TTL=128
Reply from 192.168.43.237: bytes=32 time=116ms TTL=128
Reply from 192.168.43.237: bytes=32 time=34ms TTL=128
Reply from 192.168.43.237: bytes=32 time=31ms TTL=128
Reply from 192.168.43.237: bytes=32 time=159ms TTL=128
Reply from 192.168.43.237: bytes=32 time=7ms TTL=128
Reply from 192.168.43.237: bytes=32 time=7ms TTL=128
Reply from 192.168.43.237: bytes=32 time=103ms TTL=128
Reply from 192.168.43.237: bytes=32 time=115ms TTL=128
Reply from 192.168.43.237: bytes=32 time=125ms TTL=128
Reply from 192.168.43.237: bytes=32 time=132ms TTL=128
Reply from 192.168.43.237: bytes=32 time=7ms TTL=128
Reply from 192.168.43.237: bytes=32 time=30ms TTL=128
Reply from 192.168.43.237: bytes=32 time=38ms TTL=128
Reply from 192.168.43.237: bytes=32 time=3ms TTL=128
Request timed out.
Reply from 192.168.43.237: bytes=32 time=4ms TTL=128
Reply from 192.168.43.237: bytes=32 time=6ms TTL=128
Reply from 192.168.43.237: bytes=32 time=2ms TTL=128
Reply from 192.168.43.237: bytes=32 time=63ms TTL=128
Reply from 192.168.43.237: bytes=32 time=72ms TTL=128
Reply from 192.168.43.237: bytes=32 time=88ms TTL=128
Reply from 192.168.43.237: bytes=32 time=15ms TTL=128
Reply from 192.168.43.237: bytes=32 time=4ms TTL=128
Reply from 192.168.43.237: bytes=32 time=125ms TTL=128
Reply from 192.168.43.237: bytes=32 time=135ms TTL=128
Reply from 192.168.43.237: bytes=32 time=7ms TTL=128
Reply from 192.168.43.237: bytes=32 time=159ms TTL=128
Reply from 192.168.43.237: bytes=32 time=33ms TTL=128
Reply from 192.168.43.237: bytes=32 time=32ms TTL=128
Reply from 192.168.43.237: bytes=32 time=92ms TTL=128
Reply from 192.168.43.237: bytes=32 time=103ms TTL=128
Ping statistics for 192.168.43.237:
Packets: Sent = 62, Received = 61, Lost = 1 (1% loss),
Approximate round trip times in milli-seconds:
Minimum = 2ms, Maximum = 162ms, Average = 56ms
Regards,
Mahendra Rana