Hi,
We need confirmation regarding two things about putting the device into LPDS mode.
1) Is it possible to configure multiple GPIO wakeup sources for waking up from the LPDS mode?
2) Is it possible to use the RTC wakeup and GPIO wakeup in conjunction? If yes, we would need a code sample for the same as we have tried using these two in conjunction but the device once put into sleep would not wakeup with out the sem_post even if the sleep timer (sleep(ms) function which is used for RTC wakeup) is over.
Regards
Ravija