This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 57
Part Number: WL1835MOD
Hi,
My customers want to use AM6528 and WL1835.
Customers want to use eMMC and SD Card on AM6528, so they use up only two AM65x's MMCSD(SDIO). Not enough SDIO, we can't connect WL1835(Wi-Fi) to AM65x.
Is there a way to solve this?
(For example, connect WL1835 to AM65x through QSPI.)
Regards,
Rei
Yes, WiLink8 supports SPI over SDIO interface. Although 4-bit SDIO is preferred since it offers better throughput etc.
ThanksSaurabh
In reply to Saurabh.:
>>>Yes, WiLink8 supports SPI over SDIO interface.
It is wonderful! Could you tell me about the WiLink8 SPI document and SPI Linux driver?
In reply to rei:
Hi Sauraph,
Do you have any information about SPI over SDIO?
You may refer to
Thanks
Saurabh