This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CC3135MOD: CC3135MOD

Intellectual 900 points

Replies: 1

Views: 66

Part Number: CC3135MOD

Hi,

I would like ask about CC3135mod – do You have information about time from power-on to data transmission

incl. auth etc ?

Thanks,

Jani

  • Hi Jani,

    The connection time will vary depending on the AP, security type, environment, socket type (UDP/TCP/SSL), connection policy, etc.

    For power on to firmware initialization (of network processor), you can refer to section 5.15 of the datasheet: https://www.ti.com/lit/ds/symlink/cc3135mod.pdf

    For most use-cases where this timing is critical, customers will use our intermittently connected mode an take advantage of the hibernate low-power state. Please refer to the hibernate timing sequence unless you are evaluating 1st time from hard reset.

    We break this down nicely in terms of power consumption in section 1.8 of our Network Processor Power Management guide: http://www.ti.com/lit/swra594

    For a rough indication of timing (a single data point), you can refer to Figure 38 in the same guide. This was a pretty controlled test and timing will vary as described above. The measurement was also made on the CC3235SF which will have a longer system initialize time time due to boot of M4 core. Only consider activity from NWP initialize on for CC3135.

    Best Regards,

    Ben M

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.