Radiated emissions measurements were performed in CW mode on the CC3220MODA device. Several issues were observed where the limit was exceeded for radiated emissions as follows. Note that the emissions spurs occur every 812MHz which is Fo divided by 3. Although these spurs are not harmonics of Fo, they are harmonics of Fo divided by 3. Is TI aware of any potential issues in these frequency ranges, or can TI provide some guidance on possible causes for these power level issues?
2437MHz = Fo
4062MHz (Not a harmonic) 2xFo-812, over limit.
4874MHz = 2xFo, over limit by 2.4dB
5684MHz (Not a harmonic) 2xFo+812 in spec.
6498MHz (Not a harmonic) 2xFo-812, over limit by 5.8dB
7311MHz = 3xFo, over limit by 0.9dB.
There is something every 812MHz, you cannot see it between 2437MHz and 4062MHz because it is attenuated by the high pass filter.