Other Parts Discussed in Thread: CC3120
Hi,
we use the CC3120MOD in STA mode.
I would like to confirm, the proper manner of working for our case.
The module will be used in movable device, which will move in one building_1 covered from multiple AP's, with the some SSID_1 and password_1 (but different BSSID (MAC)).
The device can move to other building_2 covered from AP's with SSID_2 and password_2 (with different BSSID's)
The usage is intermittently connected.
Connection policy is Auto + fast.
IP address allocation mode is by DHCP.
Questions:
1. Is this topology of the Wi-Fi network is possible?
2. Can I use the profiles, which can be stored in the CC3120MOD (up to 7) for purpose of a ?
profile_1 - > building_1 with SSID_1 and password_1. (MAC_11, MAC_12, MAC13,...)
profile_2 -> building_2 with SSID_1 and password_2 (MAC_21, MAC_22, MAC33,...)
profile_3 .......
..
profile_7 -> ....
If yes, I will use the API sl_WlanProfileAdd(), because custom application for delivering of the SSID and password is used.
One of the input parameters of this API is MAC address, is this value is a must?
If I have Wi-Fi network from AP's , with the some SSID and passords and different BSSID (MAC addresses), which MAC address should be used for this parameter.
Best regards,
Ilian