Other Parts Discussed in Thread: UNIFLASH, ISOW7841
Tool/software: Code Composer Studio
Hello,
I designed a custom device using CC3200.
- servicepack_1.0.1.14-2.12.2.8.bin was loaded using Uniflash.
pinmux.c
#include "pinmux.h" #include "hw_types.h" #include "hw_memmap.h" #include "hw_gpio.h" #include "pin.h" #include "rom.h" #include "rom_map.h" #include "gpio.h" #include "prcm.h" //***************************************************************************** void PinMuxConfig(void) { // // Set unused pins to PIN_MODE_0 with the exception of JTAG pins 16,17,19,20 // // // Enable Peripheral Clocks // MAP_PRCMPeripheralClkEnable(PRCM_GPIOA0, PRCM_RUN_MODE_CLK); MAP_PRCMPeripheralClkEnable(PRCM_GPIOA1, PRCM_RUN_MODE_CLK); MAP_PRCMPeripheralClkEnable(PRCM_GPIOA3, PRCM_RUN_MODE_CLK); MAP_PRCMPeripheralClkEnable(PRCM_UARTA0, PRCM_RUN_MODE_CLK); MAP_PRCMPeripheralClkEnable(PRCM_UARTA1, PRCM_RUN_MODE_CLK); // // Configure PIN_50 for GPIO Output // MAP_PinTypeGPIO(PIN_50, PIN_MODE_0, false); MAP_GPIODirModeSet(GPIOA0_BASE, 0x1, GPIO_DIR_MODE_OUT); // // Configure PIN_64 for GPIO Output // MAP_PinTypeGPIO(PIN_64, PIN_MODE_0, false); MAP_GPIODirModeSet(GPIOA1_BASE, 0x2, GPIO_DIR_MODE_OUT); // // Configure PIN_03 for GPIO Output // MAP_PinTypeGPIO(PIN_03, PIN_MODE_0, false); MAP_GPIODirModeSet(GPIOA1_BASE, 0x10, GPIO_DIR_MODE_OUT); // // Configure PIN_04 for GPIO Output // MAP_PinTypeGPIO(PIN_04, PIN_MODE_0, false); MAP_GPIODirModeSet(GPIOA1_BASE, 0x20, GPIO_DIR_MODE_OUT); // // Configure PIN_18 for GPIO Input // MAP_PinTypeGPIO(PIN_18, PIN_MODE_0, false); MAP_GPIODirModeSet(GPIOA3_BASE, 0x10, GPIO_DIR_MODE_IN); // // Configure PIN_53 for GPIO Output // MAP_PinTypeGPIO(PIN_53, PIN_MODE_0, false); MAP_GPIODirModeSet(GPIOA3_BASE, 0x40, GPIO_DIR_MODE_OUT); // // Configure PIN_45 for GPIO Output // MAP_PinTypeGPIO(PIN_45, PIN_MODE_0, false); MAP_GPIODirModeSet(GPIOA3_BASE, 0x80, GPIO_DIR_MODE_OUT); // // Configure PIN_55 for UART0 UART0_TX // MAP_PinTypeUART(PIN_55, PIN_MODE_3); // // Configure PIN_57 for UART0 UART0_RX // MAP_PinTypeUART(PIN_57, PIN_MODE_3); /*// IF THE TX AND RX PIN CONFIGURATION LINES ACTIVATED BELOW, THERE IS NO DATA AT TX PIN(GPIO_10). // Configure PIN_01 for UART1 UART1_TX // MAP_PinTypeUART(PIN_01, PIN_MODE_7); // // Configure PIN_02 for UART1 UART1_RX // MAP_PinTypeUART(PIN_02, PIN_MODE_7);*/ // IF THE TX AND RX PIN CONFIGURATION LINES ACTIVATED BELOW, THERE IS DATA AT TX PIN(GPIO_03). // // Configure PIN_58 for UART1 UART1_TX // MAP_PinTypeUART(PIN_58, PIN_MODE_6); // // Configure PIN_59 for UART1 UART1_RX // MAP_PinTypeUART(PIN_59, PIN_MODE_6); }
some part of uart_if.c
//***************************************************************************** // Global variable indicating command is present //***************************************************************************** static unsigned long __Errorlog; //***************************************************************************** // Global variable indicating input length //***************************************************************************** unsigned int ilen=1; #define UART1_BAUD_RATE 115200 #define SYSCLK1 80000000 #define CONSOLE1 UARTA1_BASE #define CONSOLE1_PERIPH PRCM_UARTA1 //***************************************************************************** // //! Initialization //! //! This function //! 1. Configures the UART to be used. //! //! \return none // //***************************************************************************** void InitTerm() { #ifndef NOTERM MAP_UARTConfigSetExpClk(CONSOLE,MAP_PRCMPeripheralClockGet(CONSOLE_PERIPH), UART_BAUD_RATE, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE)); MAP_UARTConfigSetExpClk(UARTA1_BASE,MAP_PRCMPeripheralClockGet(PRCM_UARTA1), UART_BAUD_RATE, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE)); #endif __Errorlog = 0; }
some part of main.c
void Message1(const char *str) { GPIO_IF_Set(COM_LED, mycom_led_port, mycom_led_pin, 1); UART_PRINT("\r\n .message1 called: \r\n"); #ifndef NOTERM if(str != NULL) { while(*str!='\0') { MAP_UARTCharPut(UARTA1_BASE,*str++); //MAP_UARTCharPut(UARTA1_BASE, *str++); UART_PRINT("X"); } } #endif } void LEDBlinkyRoutine() { // // Toggle the lines initially to turn off the LEDs. // The values driven are as required by the LEDs on the LP. // while(1) { Message1("ppppppp"); Message1("pppppppAAAA"); GPIO_IF_Set(RUN_LED, my_led_port, my_led_pin, 1); MAP_UtilsDelay(1000000); GPIO_IF_Set(RUN_LED, my_led_port, my_led_pin, 0); MAP_UtilsDelay(1000000); } }
When I active the lines below in pinmux.c, there is no data on UART1 tx pin:
// Configure PIN_01 for UART1 UART1_TX // MAP_PinTypeUART(PIN_01, PIN_MODE_7); // // Configure PIN_02 for UART1 UART1_RX // MAP_PinTypeUART(PIN_02, PIN_MODE_7);
BUT when I active the lines below, in pinmux.c, there is DATA on UART1 tx pin:
// // Configure PIN_58 for UART1 UART1_TX // MAP_PinTypeUART(PIN_58, PIN_MODE_6); // // Configure PIN_59 for UART1 UART1_RX // MAP_PinTypeUART(PIN_59, PIN_MODE_6);
Could you please help why I cannot configure the PIN_58 and PIN_59?
Best regards,
Onur