Hi team,
Can you comment on my customers request?
In the datasheet for the cc3220moda in chapter 5.3 there is an operating temperature of 85°C. However, the transmit duty cycle must be less than 50% to prevent the auto protection from responding.
We would like to simulate this requirement in a climate test. Therefore different transmit duty cycles have to be set at different temperatures. Especially from 75°C a maximum transmit duty cycle of 50%.
After consulting our programmers, this is not easily possible, because the data rate fluctuates and adapts to the cell load.
1. is there a possibility to set the transmit duty cycle to reach a maximum of 50%?
2. is there perhaps already software or a test environment/documentation that we can work with without the programmers having to program?
Thank you,
Franz