Tool/software: Code Composer Studio
Hi Team,
I'm using one-wire protocol (MAX31850) for Thermocouple, for reading and writing bits using UtilsDelay. My objective is to have minimum 15Micro sec delay and maximum 60 Microsec delay between 2 consecutive gpio read operation. With optimization level set to -Og it is working (able to read thermocouple output) properly but on setting optimization level to None, it is not reading properly. Let me know why it is behaving so on setting optimization to None. Earlier i used usleep for introducing delay, it was not working as expected so used UtilsDelay . Is there any other API available 2 introduce 15 sec delay.
FYR,
Development Environment : CCS V9.2.0, simplelink_cc32xx_sdk_3_40_00_05
Compiler : ARM gcc v7.2.1 (Linaro).
Regards,
Parthasarathi