This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/WL1835MOD: Wi-Fi Direct connection between Android and BeagleBone sometimes get GONegotiationFailure

Part Number: WL1835MOD


Tool/software: Linux

I try to establish Wi-Fi direct connection between Android and Beagle Bone Black Wireless running Debian 9.2 2017-10-10 4GB SD IoT image.
Sometimes it works but sometimes I get P2P-GO-NEG-FAILURE status=-1. Below I describe steps to reproduce my problem.

Firstly when I still have Internet I upgrade system and install additional dependencies which will be required later
sudo apt update && sudo apt upgrade
sudo apt install python3-pip
pip3 install --user pydbus
and I copy using scp script wifi_direct.py from here gist.github.com/.../691cdb76c68ad699b48e131490b5119d to BeagleBone.

By default BeagleBone debian configures SoftAp which conflicts with Wi-Fi direct. I disable this by setting TETHER_ENABLED=no in /etc/default/bb-wl18xx.

Note that after that DHCP server will stop running on Ethernet-over-USB interface github.com/.../32 so on the host machine we will need to assign IP addresses manually to our Ethernet-over-USB interfaces
ifconfig eth1 192.168.6.1; ifconfig eth0 192.168.7.1
then we can ssh to BeagleBone using ssh debian@192.168.6.2 or ssh debian@192.168.7.2.

I add /etc/wpa_supplicant/wpa_supplicant.conf configuration file with content

device_name=BeagleBone
device_type=1-0050F204-5
config_methods=pbc

and edit ExecStart line in /lib/systemd/system/wpa_supplicant.service to look like

ExecStart=/sbin/wpa_supplicant -u -s -O /run/wpa_supplicant -c /etc/wpa_supplicant/wpa_supplicant.conf

so this configuration file will be picked up.

Now to narrow scope of the issue I try to reproduce it using only wpa_supplicant on fresh boot.
So I boot system and make sure that after boot no wpa_supplicant is running.

$ ps aux|grep wpa_supplicant

Then I stop connman and lanuch wpa_supplicant

# systemctl stop connman
# systemctl start wpa_supplicant

After that I run attached {{wifi_direct.py}} script

python3 wifi_direct.py

It works according to following simple algorithm
1. Run P2P find.
2. Accept whatever P2P connection.
3. When other side disconnects remove P2P group.
4. Go to step 1.

From my Android phone I scan for P2P devices, try to connect to BeagleBone, then disconnect and then repeat this steps.

For some reasons after 5-15 retries I get P2P-GO-NEG-FAILURE status=-1 on BeagleBone side. Journal logs are attached. Could you please suggest what I might be doing wrongly?

Please find journal log gist.github.com/.../5740d17b211d5991a33b53ad35c22d3c and prints of my script gist.github.com/.../edd68fe87435576a6d8eca633b4822b9

  • Hi,



    I also suggest you make sure there is no hostap/wpa_supplicant that is still running in the background before you start p2p.

    In general a p2p connection failure may happen if the wifi environment is congested. If you try again, does it eventually connect?
    From your log it looks like the device was just stopped being seen:

    P2P-DEVICE-LOST p2p_dev_addr=a2:8c:fd:8b:a1:cd

    Have you tried using our standard example scripts for wifi direct?

    processors.wiki.ti.com/.../WiLink8_WLAN_Demo:_Linux

    The example scripts can be downloaded from:
    git.ti.com/.../
    under the p2p directory.

    BR,
    Eyal