Tool/software: Linux
Hi ,
I want to know which type of packet will wake up the host in wowlan stage ? for example, broadcast , EAPOL?
Is there any relevant document mentioning this?
Thanks.
Nathan Kuo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hi ,
I want to know which type of packet will wake up the host in wowlan stage ? for example, broadcast , EAPOL?
Is there any relevant document mentioning this?
Thanks.
Nathan Kuo
Hi Saurabh,
1.Wake up on any TCP packet sent to MAC 38:d2:69:c5:4e:55
iw phy0 wowlan enable patterns 38:d2:69:c5:4e:55:-:-:-:-:-:-:08:00:45:-:-:-:-:-:-:-:-:06:-:-:-:-:-:-:-:-:-:-:-:-
2.Wake up on any UDP packet sent to MAC 38:d2:69:c5:4e:55
iw phy0 wowlan enable patterns 38:d2:69:c5:4e:55:-:-:-:-:-:-:08:00:45:-:-:-:-:-:-:-:-:11:-:-:-:-:-:-:-:-:-:-:-:-
Is the above setting correct?
Nathan Kuo
Hi Nathan
1.Wake up on any TCP packet sent to MAC 38:d2:69:c5:4e:55
iw phy0 wowlan enable patterns 38:d2:69:c5:4e:55:-:-:-:-:-:-:08:00:45:-:-:-:-:-:-:-:-:06
2.Wake up on any UDP packet sent to MAC 38:d2:69:c5:4e:55
iw phy0 wowlan enable patterns 38:d2:69:c5:4e:55:-:-:-:-:-:-:08:00:45:-:-:-:-:-:-:-:-:11
Saurabh
Hi Saurabh,
Thanks for your help.
I have more questions about this.
I set the RX filter as below.
1.Wake up on any TCP packet sent to MAC 38:d2:69:c5:4e:55
iw phy0 wowlan enable patterns 38:d2:69:c5:4e:55:-:-:-:-:-:-:08:00:45:-:-:-:-:-:-:-:-:06
But the host will wake up on NBNS(UDP) packet , do you know why?
Attachment is sniffer file get from wireshark.
Please give me some suggestions.
Nathan Kuo
Hi Saurabh,
We did some experiments as follows ,
1. We set wake up on any TCP packet sent to MAC 38:d2:69:c5:4e:55
iw phy0 wowlan enable patterns 38:d2:69:c5:4e:55:-:-:-:-:-:-:08:00:45:-:-:-:-:-:-:-:-:06
2.The Windows PC connected to the same AP and then used the TCP ping tool to ping our DUT. The DUT's SoC Will be awakened
3.The Windows PC connected to the same AP and then used the ICMP ping tool to ping our DUT. The DUT's SoC Will not be awakened.
The question is whether NBNS will wake up the SoC under the TCP WoWLAN setup?
Nathan Kuo
Hi Saurabh,
Return to the original question.
We don't know why the AP Router sent the NBNS(UDP) packet and this package will wake up host.
Because our filter is only set any TCP not UDP packet
iw phy0 wowlan enable patterns 38:d2:69:c5:4e:55:-:-:-:-:-:-:08:00:45:-:-:-:-:-:-:-:-:06
Anyway, If we capture the firmware log ,do you think it will help?
Nathan Kuo
Nathan,
- Do you still receive the packet if you set filter other than TCP ?
- Do you have packet dump of the NBNS packet that is waking up the host ?
Saurabh