How do I disable the repeated-forever disconnect events?
I am piloting some special WPA-ENT station behavior, using the 'at_command' example & a python host. It is not connecting, but that's not the problem.
[WiFi: DEBUG] sent: [AT+WLanConnect=Eng-Test-Ent,,WPA_ENT,"pass","user","",PEAP0_MSCHAPv2]
[WiFi: DEBUG] recv: [OK]
[WiFi: DEBUG] recv: [+eventwlan:disconnect,Eng-Test-Ent,0x6e:0x3a:0x1e:0x83:0x8f:0x73,208]
[WiFi: DEBUG] recv: [+eventwlan:disconnect,Eng-Test-Ent,0x6e:0x3a:0x1e:0x83:0x8f:0x73,208]
[WiFi: DEBUG] recv: [+eventwlan:disconnect,Eng-Test-Ent,0x6e:0x3a:0x1e:0x83:0x8f:0x73,208]
(these events repeat once a second forever!)
Ideally I get a single "+eventwlan:disconnect" event, or a few. I see there is a set-policy to enable 'auto' reconnection, but I'm not seeing the ability to turn this off - to be full manual. I did try setting policy to 'fast' (so NOT auto), but that does not stop the repeated disconnect events. At the moment, the only way to disable these events seems to be try to connect to a FAKE non-existent ACCESS-POINT with WPA2 (not ENT) and let that fail. The 208 'reason code' means "disconnect while connecting"