Other Parts Discussed in Thread: CC3235SF
I use example from TI trigger_mode_ CC3235SF_LAUNCHXL_nortos_css for low power Wi-Fi interface. And during test found some strange behavior of SDK command sl_Send() when size of array more that 395 bytes then in debug process was crash , MCU in loop not reacted on external INT events and current consumption of board increase from 80mA to 120mA. MCU not response , only power interrupt allow to come back to normal state. When size of array less 395 bytes or equal then no problem in performance. I seen in examples for RTOS TI where array size is 1000 bytes, maybe these limits related to NON -RTOS usage only or related to power trigger mode?
unsigned char TxData[1024]={0}; //array for transmitting data
int SizeTxData=0;// size of pseudo-dynamic array for transmitting data
// SizeTxData=395;//384;//256;
statusX = sl_Send(gLocalSocketDescriptor, TxData, SizeTxData, 0);