Hi,
I have a client who has been reporting frequent disconnection of the device from the router. When I retrieved the logs I was able to notice the following string printed on the console.
[WLAN] AP disconnected on Error: 6
The definition specifies SL_WLAN_DISCONNECT_FRAME_FROM_NONAUTH_STA (6)
What could be causing this issue? It is also observed that the device by it self gets connected almost immediately after this disconnection. This entire connection disconnection event repeats it self every 10 to 15 minutes. Could you tell me what is causing this issue.
The router details to which the device is connected to is an EX7300v2 Nighthawk WiFi Mesh Extender.
Also, could you share with me a list of devices with which the CC3235SF is compatible with in order to maintain a proper connection and does not face disconnections due to power policy or some other protocol incompatibility. This is with reference to provide support to my clients.
Thank you.
Regards,
Darpan.