Hello,
I have found an strange issue on zstack communication. I am using zstack varsion 2.5.1a for cc2530 chip and one of the examples called SampleApp. I found out that sometimes the delay after function AF_DataRequest (message is seen with packet sniffer) can be as long as 300 - 500 ms, when it is normally about 20-50 m. I am doing a test where large amount of data packets is sent through network and these kind of delays are not wanted. Same issue occurs zstack earlier version 2.5.0. The delay is in Coordinator's transmit. End Device seems to transmit OK.
It looks like the situation occurs when radio signal gets weak, for example there is some obstacle between antennas or suchlike. When system goes to "slow-mode" it will continue slow even if signal level gets back to good. SystemReset corrects the situation back to normal.
Has anyone had this kind of problems, and is there any solutions of this?
Thanks to all,
Risto