Hello all,
I am working with the design files of the TIDM-LOWEND-IHD and I found here the HEX files for the CC2530 coordinator and end device that should be used with the IHD. I programmed this files and could establish connection between them, but I can only send active power in one direction, from coordinator to end device. I would like to use this code and send also other variables that I am measuring, but as I have no access to the source code for the CC2530 devices I haven't been able to do it. Also, I need this link to be bidirectional.
The design files that I am using can be found here, http://www.ti.com/lit/zip/tidc258,