This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531EM-IOT-HOME-GATEWAY-RD: What is (STATUS=4) ? in BIND not successful msg in LINUX HA Gateway application

Part Number: CC2531EM-IOT-HOME-GATEWAY-RD
Other Parts Discussed in Thread: CC2531, CC2650

hi i'm using CC2531 as ZNP and running Linux HA Gateway App on pi,

When i bind the ON/OFF Cluster Endpoint  in ZED (cc2650) to ZC, i get the following msg:

Binding source selected

Sending bind command

binding source_address 0x124b00......40  endpoint  0x08

binding destination_address 0x124b00...fa  endpoint 0x3

sent to NWK_MGR: len=36, cmd_id=26, subsystem=18

Raw= 24:00:  ....

received from NMK_MGR: len=6, cmd_id=0, subsystem=114

Raw=06:00.....

Calling confirmation callback

comm_device_binding_entry_request_confirm: Received ZIGBEE_GENERIC_CNF

comm_device_binding_entry_request_confirm: Status SUCCESS.

received from NWK_MGR: len=21, cmd_id=27, subsystem=82

Raw:15:00:............

comm_device_binding_entry_rsp_ind :  Received NWK_MGR_CMD_ID_T__NWK_SET_BINDING_ENTRY_RSP_IND

Bind/Unbind not successful (status=4)