This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2520: CC2520 interface with CC2592

Part Number: CC2520
Other Parts Discussed in Thread: CC2591, CC2592, , CC2530

Will CC2592 work with CC2520? Can i interface CC2592 with CC2520 following similar reference design of CC2520 + CC2591 i.e the way output of CC2520 is connected to input of CC2591.

Will there be any RF performance issue? 

And also curious to know what is the maximum output power can be achieved at antenna connector.

Thanks,

Biswas

  • Hi,

    Yes, you can start with CC2520+CC2591 design. Replace CC2591 circuit with the CC2592 circuit (refer to CC2530+CC2592 Design for CC2592 Circuit).
    You may need to adjust the matching in between CC2520 and CC2592 on Prototypes for optimum performance.
    Please refer to SWRA465 for CC2530+CC2592 performance. We would expect a similar performance from CC2520+CC2592 combination also.

    Thanks,
    PM