Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538-CC2592EMK: Maximum no. of devices allowed in zigbee network.

Guru 14820 points

Part Number: CC2538-CC2592EMK
Other Parts Discussed in Thread: CC2650, Z-STACK, CC2538

Hello,

I am using cc2538 as cordinator as well as router and cc2650 as end devices. And using z-stack 3.0 for cc2538 and z-stack 1.2.2a for cc2650. I am using coordinator as znp and connected to Raspberry pi with z-stack linux gateway.

1) Does both the stacks are based on zigbee pro features?

2) what is the max no. of routers can be connected to coordinator directly?

3) what is the max no. of end devices can be connected to coordinator directly?

4) what is the max no. of end devices can be connected to a router?

5) what is the max no of end devices/routers can be there in a network(overall network size)?

6)Is it possible to increase max node depth to value greater then 5?