Part Number: CC2538
Tool/software: TI-RTOS
Hi
I want to flash firmware(.bin) in CC2538 using "sblAppEx".
I got below error 8 time out of 10 tries.
Erasing flash ... DONE
Writing flash ...
SBL Progress: 0%
SBL Progress: 1%
SBL Progress: 2%
SBL Progress: 3%
SBL Progress: 4%
SBL Progress: 5%
SBL Progress: 6%
SBL Progress: 7%
SBL Progress: 8%
SBL Progress: 9%
SBL Progress: 10%
SBL Progress: 11%
SBL Progress: 12%
Error during flash download.
- Start address 0x00203D40 (page 7).
- Tried to transfer 64 bytes.
- This was transfer 246.
any solution for this?
Note:
1) I dont want to use any tool. i want to do by any application.
2) I have generated .bin file using ccs.
Regards,
Prerak.