This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/CC2530: IR Receiving using input capture feature of timer

Part Number: CC2530

  //Initialisation;
  void irLearnerInit(uint8 irType)
  {
    //Timer Clock Source = 32MHz
    CLKCONCMD &= 0x80;
    
    //Timer-1 priority over uart
    P2DIR |= BV(7);
    //Timer-1 channel0 alternate2 i.e. P1_2
    PERCFG &= ~BV(4);
    
    P1INP |= BV(2);
    P1SEL |= BV(2);
    P1DIR &= ~BV(2);
    
    //timer1 channel0 interrupt mask
    T1CCTL0 |= BV(6);
    
    //rest channel interrupt disabled
    T1CCTL1 &= ~BV(6);
    T1CCTL2 &= ~BV(6);    
    T1CCTL3 &= ~BV(6);
    T1CCTL4 &= ~BV(6); 
    
    T1OVFIM = 0;
    T1STAT &= ~BV(0);
    
    //Enables interrupt
    T1IE = 1;
    T1IF = 0;
    EA = 1;
    T1CCTL0 &= ~BV(2);
    
    //interrupt on all edge
    T1CCTL0 |= BV(1);
    T1CCTL0 |= BV(0);
    
    //Timer1 clock frequency 1MHz
    T1CTL |= 0x08;
    
    //free-running mode active
    T1CTL |= 0x01;
  }

  HAL_ISR_FUNCTION( IRisr, T1_VECTOR )
  {
    HAL_ENTER_ISR();
    if(T1STAT &  BV(0)) //overflow interrupt occur
    {
      T1STAT &= ~BV(0); //clear interrupt flag
      irProcessInterrupt();
    }
    T1IF = 0;
    CLEAR_SLEEP_MODE();
    HAL_EXIT_ISR();
  }
  
  void irProcessInterrupt(void)
  {
    LED = ~LED; 
    irRcvBuff[pulseCount]  = T1CC0H;
    pulseCount++;
    irRcvBuff[pulseCount]  = T1CC0L;
    pulseCount++;
    timeoutCountStart = 1;
  }

Tool/software: WEBENCH® Design Tools

I have successfully implemented the IR blaster using Timer 1 and Timer 3.

But now I want to implement IR Learner but don't know how to setup for it.

I know little bit about Timer1 & Timer 3 capture but don't know exactly what to do.

Can anybody help me with this??