Other Parts Discussed in Thread: Z-STACK, , LAUNCHXL-CC26X2R1
Hello,
I am using a custom designed board which uses the cc2652r and I am not able to read or write anything on to the external flash in the Z-stack Application layer. I intend to use the Flash for OTA. The Flash is being detected in the bim project and factory image is copied.
SDKs used:
1) simplelink_cc26x2_sdk_2_20_00_36
2) simplelink_zigbee_sdk_plugin_2_20_00_06
Example Project on which Custom application is developed: zed_switch_ota .(built on IAR EW Arm 8.30.1)
Below is the Flash Pin Configuration modified as per custom board that we designed.
Default Configuration | DIO/IOID | Custom Configuration | DIO/IOID |
CC26X2R1_LAUNCHXL_SPI_FLASH_CS | IOID_20 | CC26X2R1_LAUNCHXL_SPI_FLASH_CS | IOID_10 |
CC26X2R1_LAUNCHXL_SPI0_MISO | IOID_8 | CC26X2R1_LAUNCHXL_SPI0_MISO | IOID_9 |
CC26X2R1_LAUNCHXL_SPI0_MOSI | IOID_9 | CC26X2R1_LAUNCHXL_SPI0_MOSI | IOID_11 |
CC26X2R1_LAUNCHXL_SPI0_CLK | IOID_10 | CC26X2R1_LAUNCHXL_SPI0_CLK | IOID_12 |
have modified the SPI pin settings in
C:\ti\simplelink_cc26x2_sdk_2_20_00_36\examples\rtos\CC26X2R1_LAUNCHXL\ti154stack\common\boards\CC26X2R1_LAUNCHXL\CC26X2R1_LAUNCHXL.h
C:\ti\simplelink_zigbee_sdk_plugin_2_20_00_06\examples\rtos\CC26X2R1_LAUNCHXL\zstack\common\boards\CC26X2R1_LAUNCHXL\CC26X2R1_LAUNCHXL_OAD.h