Part Number: CC2531
Other Parts Discussed in Thread: Z-STACK
Hi all!
========================
System:
Based on TI_Z-stack_HA1.2.
Sniffer:
Ti CC-2531 (+TiWsPc) + WireShark
========================
During integration of the IAS_ACE KeyFob to our system, I have faced with an issue, that the gateway server doen't recieve any ARM or Emergency commands.
While the IAS_ZONE Devices are working perfectly.
Let's consider the Z-Stack Linux Gateway Application Programming Interface document (for ex, v.1.1., May 2014).
The gateway should process the 9.6.1 DEV_ACE_ARM_REQ_IND, as far as I understood.
Consider (gatewaysrvr.c)
static ZStatus_t gwHandleServerIndPbCb( zclIncoming_t *pInMsg ),
where
case ZCL_CLUSTER_ID_SS_IAS_ACE:
status = processIasAceClusterCmdInd( &srcAddress, pInMsg );
break;
is processed.
It comes there from
static ZStatus_t zcl_HdlIncoming( zclIncoming_t *pInMsg )
I have added there logs:
uiPrintfEx(trUNMASKABLE, "zcl_HdlIncoming: ClusterID: %d\n", pInMsg->msg->clusterId);
If the device is IAS-Zone (for example, WaterLeackage sensor), I can see something like
"
[15:41:21.362,261] [GATEWAY/HNDL] UNMSKBL: zcl_HdlIncoming: ClusterID: 1280
[15:41:21.362,347] [GATEWAY/HNDL] UNMSKBL: zcl_HdlIncoming: Processing abstracted ZCL command
"
So everything is ok.
While if I am sending ACE commands (Arm: All Zones, Disarm, Arm Day / Home Zones Only) from my KeyFob, I can see them coming from sniffer,
while they are not processed by
static ZStatus_t zcl_HdlIncoming( zclIncoming_t *pInMsg ).
P.S.
If I am right, I should Consider our system (ZNP) the IAS_ACE server, while the KeyFob is IAS_ACE device.
KeyFob has been: Successfully connected (enrolled, clusters have nee read etc..)
In gateway-config.tlg:
// - supporting as server (accepting client to server commands):
clusterlist CombinedInterfaceInputClusters { basic, identify, IasAceClusterId }
string was unchanged.