Other Parts Discussed in Thread: Z-STACK, , CC1352P, CC2652R, CC2538
Hello,
I have a zigbee network with a CC2530 (Z-Stack 1.2.2) device as zigbee coordinator (using zigbee API) and 30 CC2530 (Z-Stack 3.0.1) devices as zigbee router. The routers report periodically some attributes (every 1-2 mins) and they ask, also periodically, if there is a new firmware (OTA Upgrade, every 10 mins with jitter).
I see from a log file that frequently the coordinator can't send the OTA Upgrade response message because the firmware returns the error code 0xCD (nwk no route). But the reports from the router are ok and I can send commands.
On the sniffer, I can see that the response message is not sent, but the coordinator doesn't try to restore the route with a Route Request. In fact the route request messages that I see seem to be not related. I also notice that the coordinator has only 17 neighbors, but all the 30 devices are in 2 meters range.
Anyone can help me to understand this behaviour?
Thanks,
Antonio