Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: GPP don't deliver GPDF in tunnel mode.

Part Number: CC2652R

Hi Team,

Customer uses green power function with SDK(version 3.10). In customer mesh network, GPP don't deliver GPDF.  GPP device is generic router. I can't reproduce this issue, customer will provide more details later.

http://dev.ti.com/tirex/explore/node?node=ACZCmxTLN0qLaDEkki-bLQ__pTTHBmu__LATEST

  • Hardware: three hardware board of LaunchpadCC2652

    Plartform: SDK V3.10.00.53

    Project:zcl_light_sink, zr_genericapp, gpd_sw

           For the project zr_genericapp, I have change the button behavior to enable/disable the commission mode(gp_SetProxyCommissioningMode) by button click.

    step1: the Light Sink and another routing device are in the same network,

    step2: put the Light Sink(gp_SetSinkCommissioningMode=TRUE) and Router(gp_SetProxyCommissioningMode=TRUE) in commissoning mode

    step3: GPD send the On/Off GPDF to trigger the pairing prcess (packet number 76 - 85, please reffer to the attachment "gp")    

    step4: disable  the GP commissioning mode on the Light Sink and the Proxy.

    step5: the GPD Switch can toggle the Light Sink LED(direct mode)

    I have repeat the steps sevel times, but found that the network is always be in the direct mode.

    how to establish a tunnel mode link between the Sink and the GPD?

    gp.zip

  • Hi,

    According to the state machine for GP Proxy Basic, the GPPB will not enter Proxy commissioning mode until it receives GP Proxy Commissioning Mode (Action==enter).

    Please see the callback that handles the GP Proxy Commissioning mode command: zclGp_GpProxyCommissioningModeCB.

    Can you try UI_SetGPPCommissioningMode instead of gp_SetProxyCommissioningMode?



    Regards,
    Toby
  • Hi,Toby,

    thank you for you reply.

    I modify the code in the zclGenericApp_processKey() as follow:

    static void zclGenericApp_processKey(uint8 keysPressed)
    {
        zstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq;
        //Button 1
        if(keysPressed == KEY_LEFT)
        {
            if(ZG_BUILD_COORDINATOR_TYPE && ZG_DEVICE_COORDINATOR_TYPE)
            {
    
                zstack_bdbStartCommissioningReq.commissioning_mode = BDB_COMMISSIONING_MODE_NWK_FORMATION | BDB_COMMISSIONING_MODE_NWK_STEERING | BDB_COMMISSIONING_MODE_FINDING_BINDING;
                Zstackapi_bdbStartCommissioningReq(appServiceTaskId,&zstack_bdbStartCommissioningReq);
            }
            else if (ZG_BUILD_JOINING_TYPE && ZG_DEVICE_JOINING_TYPE)
            {
                zstack_bdbStartCommissioningReq.commissioning_mode = BDB_COMMISSIONING_MODE_NWK_STEERING | BDB_COMMISSIONING_MODE_FINDING_BINDING;
                Zstackapi_bdbStartCommissioningReq(appServiceTaskId,&zstack_bdbStartCommissioningReq);
            }
    
    
    
    
    
            //add
            static uint8 tmpSta = 0;
    
            if(zclport_isAlreadyPartOfNetwork(appServiceTaskId)){
                if(tmpSta){
                    Board_Led_control(board_led_type_LED1, board_led_state_ON);
    
                    #if defined(BOARD_DISPLAY_USE_UART_EXT)
                        genericApp_UART_write("ON\r\n", sizeof("ON\r\n"));
                    #endif
    
                    zclGpProxyCommissioningMode_t cmd;
                    cmd.options = GP_COMM_OPT_ACTION_MASK;
                    cmd.srcAddr = 0x0000;
                    zclGp_GpProxyCommissioningModeCB(&cmd);
                }else{
                    Board_Led_control(board_led_type_LED1, board_led_state_OFF);
    
                    #if defined(BOARD_DISPLAY_USE_UART_EXT)
                        genericApp_UART_write("OFF\r\n", sizeof("OFF\r\n"));
                    #endif
    
                    zclGpProxyCommissioningMode_t cmd;
                    cmd.options = 0;
                    cmd.srcAddr = 0x0000;
                    zclGp_GpProxyCommissioningModeCB(&cmd);
                }
            }
    
            tmpSta ^= 1;
        }
    }

    but the problem still exists.

  • It appears that the GPPB needs to update its proxy table in order to tunnel GPDFs. I think the issue here is that the GPPB is not updating its proxy table.

    According to the state machine, after a successful GPD to GPCB pairing, the GPCB should send a GP Pairing command (gpPairingCmd_t), which will make the GPCB update its table command. This would happen regardless if GPPB is in operational or commissioning mode.

    I need to further investigate to figure out why this is not happening.

  • I've reported the issue, and our team is looking at the best way to fix the issue.