Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: Z-STACK
Tool/software: Linux
Dear all,
I'm try to setup the Linux Gateway on a RPi3 model B+ and using the LAUNCHXL-CC26X2R1 as ZNP coordinator, I've read some post over the forum but I need some starting point in order to go straigght and understand precisely all the details.
As a first step I'm start from the:
Z-Stack Linux Gateway - Quick Start Guide
so I've did the very first step:
- sudo apt-get update
- sudo apt-get upgrade
-sudo apt-get install psmisc
- sudo apt-get install dos2unix
Then I'm try to install also the protobuf compiler:
sudo apt-get install autoconf automake libtool curl make g++ unzipapt-get install protobuf-c-compilergit clone github.com/.../protobuf.gitcd protobuf./autogen.sh./configuremakemake checksudo make installsudo ldconfig # refresh shared library cache.
but every time this fails with error :
dpkg: unrecoverable fatal error, aborting:
files list file for package 'apt' is missing final newline
E: Sub-process /usr/bin/dpkg returned an error code (2)
at the moment by means of the classical apt-get is not possible to install it, so download the protobuf-cpp-3.8.0.tar.gz from the site and then perform a manual compile from source, it take approx 2h but it work without problem.
download the source file from https://github.com/protocolbuffers/protobuf/releases
protobuf-cpp-3.8.0.tar.gz
into a RPi folder (e.g. /home/pi)
unpack it with:
tar -xvzf protobuf-cpp-3.8.0.tar.gz
then:
cd protobuf-3.8.0
./configure
make
sudo make install
sudo ldconfig
to test if properly installed follow the example tutorial at this link: https://developers.google.com/protocol-buffers/docs/tutorials
pick the one you prefer and follow the tutorial.
The next step is how to install the Linux gateway on RPi3 model B+ with Raspbian GNU/Linux 9 (stretch) 32 bit operating system and know if someone have succesfully did it.
To get the source to install one way is to install the Zigbee_3_0_Linux_Gateway_1_0_1.exe file on a Windows machine, then by a FTP tool (WinSCP) trasfer the source code to the RPi, now the question is if someone have tested it and if exist some port from BBB to the RPi3.
Thank!