This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630: Is it okay to use a internal LDO mode with Interanl DC-DC H/W configuration?

Part Number: CC2630


Hi,

A customer built a PCB with a internal DC-DC regulator configuration like below.

but for some reason, the customer wants to use a internal LDO configuration without chaing the H/W.

so question is..

is it okay to use the internal LDO configuration with just configuring  CCFG like below  without H/W change(10uH is mounted between DCDC_sw pin and Vddr pins)?

//#define SET_CCFG_MODE_CONF_DCDC_RECHARGE 0x1 // Do not use the DC/DC during recharge in powerdown
//#define SET_CCFG_MODE_CONF_DCDC_ACTIVE 0x1 // Do not use the DC/DC during active mode