I have a CC1352P-2 LaunchPad, I'm using the Simplelink_cc13x2_26x2_sdk version 3.20.0.68 (which is the latest). I'm trying to create the "ADC Data Streamer" example project.in Sensor Controller Studio to try on this board.
When I create the project, it asks me to select an SDK. However my SDK is not one of the selections, and it won't let me enter my SDK, I'm forced to select from a list. The latest SDK it supports is Simplelink_cc13x2_26x2_sdk version 3.10.01.11. I have version 3.20.0.68.
BTW, I have installed all available Sensor Controller Studio patches.
How can I get Sensor Controller Studio to use my SDK? I could downgrade to an older SDK (if it's still available for download) but I prefer to use the latest SDK.
Thanks,
Tim