Last Updated: Oct. 21st 2019. Fix is now available.
Known issue:
DMM-782 |
DMM ZR stops core Zigbee functionality after 1-4 hours with steady traffic |
Affected:On the SIMPLELINK-CC13X2-26X2-SDK 3.30.00.03, the DMM Zigbee Router + Bluetooth LE Peripheral example has a known stability issue where the Zigbee functionality may stop after several hours of activity.Description:
- CC13x2 / 26x2 SimpleLink SDK 3.30.00.03 DMM Zigbee Router + BLE Peripheral configuration.
Not Affected:
- Previous versions of the SDK are not affected.
- Other Zigbee + BLE DMM configurations are also not affected.
Fix: Request access to the patch installer here, then apply the patch to an existing 3.30 SDK installation:
Alternately you may also continue to develop with the previous releases that support DMM Zigbee router + BLE Peripheral configuration: