This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/CC2652R: Issue of SKD 3.30 : There is a Wild Pointer in function "zclParseInDiscCmdsRspCmd" in zcl, that will cause Z-stack crash.

Part Number: CC2652R
Other Parts Discussed in Thread: Z-STACK

Tool/software: WEBENCH® Design Tools

When a ZCL_CMD_DISCOVER_CMDS_RECEIVED_RSP or ZCL_CMD_DISCOVER_CMDS_GEN_RSP was received and parsed in zclParseInDiscCmdsRspCmd,  the z-stack will crash. The pointer "pDiscoverRspCmd->pCmdID" has not been assigned to allocated buffer. It  can be fixed like this. 

This issue is appearing in SDK 3.30, SDK3.20 , Z-stack 3.0.2

static void *zclParseInDiscCmdsRspCmd( zclParseCmd_t *pCmd )
{
  zclDiscoverCmdsCmdRsp_t *pDiscoverRspCmd;
  uint8_t *pBuf = pCmd->pData;
  uint8_t numCmds = ZCLDISCRSPCMD_DATALEN(pCmd->dataLen);  // length of command ID variable array

    // allocate memory for size of structure plus variable array
  pDiscoverRspCmd = (zclDiscoverCmdsCmdRsp_t *)zcl_mem_alloc( sizeof ( zclDiscoverCmdsCmdRsp_t ) +
                    ( numCmds * sizeof(uint8_t) ) );
  if ( pDiscoverRspCmd != NULL )
  {
    uint8_t i;
    pDiscoverRspCmd->discComplete = *pBuf++;
    pDiscoverRspCmd->numCmd = numCmds;
    pDiscoverRspCmd->pCmdID = (uint8_t*)( pDiscoverRspCmd + 1 ); //set pCmdId pointer, fixed by luoyiming 2019-10-18

    for ( i = 0; i < numCmds; i++ )
    {
      pDiscoverRspCmd->pCmdID[i] = *pBuf++;
    }
  }

  return ( (void *)pDiscoverRspCmd );
}