I am trying to read the state of the GPIO pins while running the Bootloader in UART mode. I am attempting to test the GPIO pins for stuck-at conditions on an In-circuit tester by doing COMMAND_MEMORY_READ with the bootloader from the GPIO_DATA registers, but all I get are 0s, even when the GPIO pins are driven to logic high. Is there some setup I need to do to make the GPIO module come to life? Everything is at RESET default. I know the Bootloader is working because I am able to erase and program the flash and get predictable CRC32s. Are the GPIO registers even available to me with the bootloader? If not, let me know so I don't keep attempting something that won't happen.