This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

RE: CCS/CC1352R: I2C pins on collector_SM and sensor_SM example codes

Intellectual 920 points

Replies: 3

Views: 128

Hi Toby Pan,

Thank you for reply.when I am tryong to change I2C pins i could not able to change in sysconfig file. If I need to config another pin then I have to set USE HARDWARE as NONE .But I cannot able to change it.  can you please let me know how to change default pins of  uart,I2C and SPI

Regards,

NIHARIKA

  • Hi,

    As an example, can you specify which pins you would like to use for I2C?

    That way I can try to reproduce your issue and find a potential solution.

    Regards,
    Toby

  • In reply to Toby Pan:

    Hi,

    1.For I2C I need to use  SCL-IOID_6,SDA-IOID_5

              2.UART: RX-IOID_21

                              TX-IOID_22

              3.SPI_FLASH_CS: IOID_14

                MISO:IOID_18

               MOSI:IOID_19

               CLK;IOID_20

    Regards,

    Niharika

  • In reply to LAKSHMI NIHARIKA Raviprolu73:

    For I2C, you don't need to select "Use Hardware" as none. That is just a suggestion because this DIO6 is mapped to the red LED on the launchpad. Remove the Red LED in this case ("TI DRIVER APPS" --> "LED").

    For UART, the first UART instance provided by default is for the Display. You can create a new UART instance and select the pins you want to use.

    For SPI, DIO14 was used by BTN-2 (BTN_RIGHT) on the launchpad, so you will need to remove this ("TI DRIVER APPS" --> "Button").

    Currently you will see build errors because the examples use launchpad hardware (CONFIG_BTN_RIGHT, etc).
    Feel free to modify the code to fit your project use case.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.