Other Parts Discussed in Thread: FLASH-PROGRAMMER, Z-STACK,
Hi Team,
The customer is experiencing below issue and needs your help.
1. Customer burned the boot on the CC2530 (path: C:\Texas Instruments\ZStack-CC2530-2.5.1a\Projects\zstack\Utilities\BootLoad\CC2530). He fully configured according to the Serial Boot Loader For CC253x SoC document. He burned the app with sbdemo. After the burning is finished, the traffic light is always on. But after the restart, the red light keeps flashing. Customer checked the boot code and it seemed to always return false in the sbImgValid function. He looked at the values of 0090~0091 and 0092~0093 in GenericApp.bin are the same (see the figure below). He would like to know why?
2. Customer doesn't want to use the button to jump, he wants to jump to the app after power-on. Is it OK to change the value of SB_UART_DELAY?