Other Parts Discussed in Thread: SYSCONFIG
Hi Team,
1. If I set POLL RATE to zero for battery powered devices, will it be able to rejoin ZC network without problem?
Regards,
Walter
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Walter,
Yes, if the POLL RATE is disabled after the commissioning process, the ZED should still be able to rejoin the ZC network.
Best Regards,
Marlyn
Hi Marlyn,
Thanks, currently we are setting POLL RATE to zero in config so it is not after commissioning.
By right, we should set to non-zero first in config then commission. Then, set poll rate to zero.
By the way, we are using sdk 310 zed sample sw code.
Regards,
Walter
Hi YK,
What is the problem if we set poll rate to zero before commissioning, then losses connection. It cannot re join back?
Regards,
Walter
Walter,
I was under the impression you were using SDK 3.4, my apologies.
For SDK 3.1, if you set the POLL RATE to 0 in SysConfig there should be no problem with the ZED rejoining the network.
Best Regards,
Marlyn
Hi Marlyn,
We are not using sysconfig but I think we can set poll rate = 0 in zstack config.
Regards,
Walter
Hi Walter,
If you set POLL RATE to zero in zstack_config.h, the ZED will still be able to rejoin the network.
Best,
Marlyn