Hi all,
I am desiging e zigbee znp project.
I am designing a zigbee znp project with CC1352.
I am designing the electrical drawing based in the CC1352 launch pad.
I have the questions:
1-) I am checking that the CC1352 launch pad has 3 RF channels: RF_x_2_4GHZ (2.4 GHz), RF_x_SUB_1GHZ (sub 1 GHz) and TX_20DBM_x. I need to use this 3 RF channels for my zigbee project ? Which of these RF channels I must to use in my zigbee project ? The firmware that I will use is the znp for CC1352
2-) I am checking that el el CC1352 Launchpad has a external flash memory mx25r8035fhuilo. I can remove this memory of my design? If this memory is removed of the design the znp firmware working?
Sincerely, Thanks very much. Best Regards
3-) There are differents CC1352 launchpad, what is the better for my zigbee project? For customize it