This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: ZNP sending unknown command

Part Number: CC2652R

A user noticed that the CC2652R ZNP with the SimpleLink SDK 4.10.00.78 is sending an unknown command. It also happens with 3.40.00.02 but does not seem to happen with 3.30.00.03.

This is the received byte sequence: [254,5,69,159,247,57,132,10,235,116]

Which translates to subsystem 5 (=ZDO) and command ID 159. I cannot find this command in the ZStack ZNP documentation nor source code.

What command is this?