Other Parts Discussed in Thread: Z-STACK
The receiver which is 2 to 1 transmitter, reception receives the same packet.
How long is variation of setting of interrupt flag of 2 receivers ?
regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi takenari,
Please clarify what exactly you are trying to achieve and if you are evaluating a certain stack solution. For example, in Z-Stack communication the receiver supplies a MAC ACK in 2 ms followed by a ZCL response (if necessary) after 20 ms. Stack responses vary based on the amount of processing that must be performed to determine if and how to respond.
Regards,
Ryan