Other Parts Discussed in Thread: Z-STACK
Tool/software: TI C/C++ Compiler
Hello,
I m working on Zstack 1.2.2a with the CC2530 module, I have a problem
1) when I use sleep mode it will not send data to the co-coordinator and when I disable sleep mode it will send data to the co-ordinator.
my code structure is,
Initialise Pins()//init pins
Reload Timer for 10 sec()//init reload timer
in Reload timer event
osal_pwrmgr_device(PWRMGR_ALWAYS_ON); //to wake up the device from sleep mode
Send_data to coordinator();//send data to coordinator
osal_pwrmgr_device(PWRMGR_BATTERY);//for sleep mode
I m using the following code for sending data from End device to the co-ordinator,
static void SPIKE_send_coordinator(uint8 * data,uint16 data_len)
{
GenericApp_DstAddr.addrMode = (afAddrMode_t)Addr16Bit;
GenericApp_DstAddr.endPoint = GENERICAPP_ENDPOINT;
GenericApp_DstAddr.addr.shortAddr = 0x0000;
if (AF_DataRequest( &GenericApp_DstAddr, &sampleTemperatureSensor_TestEp,
GENERICAPP_CLUSTERID,
data_len ,
data,
&GenericApp_TransID,
(AF_DISCV_ROUTE | AF_ACK_REQUEST), AF_DEFAULT_RADIUS ) == afStatus_SUCCESS ) //hitesh
{
}
}
For Sleep mode, I m using the following code,
osal_pwrmgr_device(PWRMGR_BATTERY);//for sleep mode
osal_pwrmgr_device(PWRMGR_ALWAYS_ON); //to wake up the device from sleep mode
DPOLL_RATE=0 // in config file I use
In Preprocessor, I have used
Powersaving
Please Please help me I m doing the same thing for 15 days but the problem as it as.
Thanks in advance