Other Parts Discussed in Thread: CC1352R
Hi TI !
I need to Cloning Z-Stack Network Properties from the CC1352-ZNP device.
Please, I have checked the documentation, if is possible please, check my practical problems / questions below.
There are some things not clear for me from the documentation.
Question 1-):
1-) Which one the MT command for read Z-Stack Network Properties?
If the answer is: SYS_NV_READ, I have the following problems:
Problem 1-)
I am sending via UART to my CC1352-ZNP the SYS_NV_READ command for to read ZCD_NV_EX_NWK_SEC_MATERIAL_TABLE.
I am sending:
0xFE 0x08 0x21 0x33 0x01 0x00 0x07 0x00 0x00 0x00 0x00 0x0C 0x10
The answer from the CC1352-ZNP:
0xFE 0x02 0x61 0x33 0x07 0x00 0x57
Question 2-)
2-) I did expect to get the a data stream of 12 bytes. Why I can't get the 12 bytes readed fron the NV memory?
Question 3-)
Which one the MT command for read ZCD_NC_PANID?
Which is the command correct format?
Thank you very much, Best regards