This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 0
Views: 110
These guidelines are intended to provide a reference for all stages of development using TI Thread connectivity products.
Step 0: Learn the technology
Step 1: Pick your device
Step 2: Download necessary software
Step 3: Begin software development
Step 4: Deep-dive into documentation
Step 5: Design your hardware
Step 6: Certification and production
Also see the ‘Common Development Questions’ section at the end.
Not sure which connectivity technology to use? Check out the Wireless Connectivity Technology Selection Guide!
Thread CLI Project Zero
Get started with Thread by forming and commissioning a network using the Command Line Interface
Thread Border Router Setup
Setup a Thread Border Router for off-mesh route capabilities.
DMM Fundamentals
Dynamic Multi-protocol Manager (DMM) allows multiple wireless stacks to coexist and operate concurrently on a single radio
Sensor Controller Fundamentals
How to use the Sensor Controller Studio and GUI tool
RTOS Concepts
A general overview of concepts used in Real-Time Operating Systems such as task/threads, scheduling, semaphore. Start here to learn about TI-RTOS and POSIX.
SysConfig Tool Basics
SysConfig is tool to help you configure your SimpleLink applications, generating source files for TI Drivers and software libraries
Common Development Questions
Start with the Out of Box Experience! This demo helps you learn about your LaunchPad and run your first application. After that, start to learn about the different features and software libraries we provide on SimpleLink Academy.
It is recommended that users start with one of the various development examples provided in the SDK.
The TI Drivers Runtime APIs provide basic usage summaries and examples for each peripheral, and additional TI Drivers examples are provided for each device inside the examples/<rtos>/<LaunchPad>/drivers folder of your SDK.
Use the CCSTUDIO IDE to build, load, and debug code. To program a binary image on a 2.4 or Sub1-GHZ device, refer to either FLASH-PROGRAMMER or UNIFLASH.
Find out more about the SimpleLink security features available on each stack with these White Papers.
Design reviews can be requested for Sub-1 GHz, 2.4 GHz, and Wi-Fi hardware.
The E2E Wireless Connectivity forum is the go-to source for help throughout every step of the design process.
E2E is a public forum with questions and answers posted by TI engineers and knowledgeable community members to help users quickly solve their design issues. Search a few keywords to see resolved questions, or you can ask a new question!
--------------------------------------------------------------------------------------------------------- Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------------------------------
---------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.---------------------------------------------------------------------------------------------------------