This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 21
Views: 178
Part Number: CC2530
Several devices that were apparently joined with the ZNP were not reported in the device list.
9747 2020-11-08 18:06:19.582029 00:12:4b:00:10:22:82:77 → 00:0d:6f:00:12:a0:cc:f8 IEEE 802.15.4 27 Association Response, PAN: 0xeb67 Addr: 0x099f 9789 2020-11-08 18:06:36.820021 00:12:4b:00:01:dd:7a:d7 → 00:0d:6f:00:12:19:9e:48 IEEE 802.15.4 27 Association Response, PAN: 0xeb67 Addr: 0x9584 9947 2020-11-08 18:08:53.014896 00:12:4b:00:10:22:82:77 → 00:0d:6f:00:12:a0:cc:f8 IEEE 802.15.4 27 Association Response, PAN: 0xeb67 Addr: 0x099f 9989 2020-11-08 18:09:03.594017 00:12:4b:00:10:22:82:77 → 00:0d:6f:00:12:a0:cc:f8 IEEE 802.15.4 27 Association Response, PAN: 0xeb67 Addr: 0x099f
After checking the logs, I did further attempts to allow association did not seem to set "Association Permit: True".However, I ended up noticing that I could not longer do onoff requests for the TI SampleLights neither.
In the attached zip files, you'll find the HEX file read back from the CC2530 after the Gateway/ZNP became in responsive as well as difKK.txt listing the differences with the loaded fw.DbHistoryFull holds the versions of the csv files as the network was extended (it is now automatic), the timestamp in the name of the file should be close (less than a few seconds) to when the CSV file was updated.pcap files are also included, 'lastkeys.log' has the network key, seriallog.txt.7 holds the serial communication with the CC250 .
Hopefully this helps to identify the cause for these two issues, and hopefully that leads to fixes.
AssocNonReported_ZNP_KO.zip
--Electronics & Software Engineer in France
I would recommend against adding devices to the list based on Association Responses and instead wait for the Device Announce that proves the device has received the correct NWK key. Parsing ZDP_NonResponsive.hex NV items only shows 0x099F existing as a deleted item. We have discussed ZNP non-responsiveness in some of your other E2E threads.
Regards,Ryan
To better aid the community, please click on the "This Resolved my issue" button whenever a post answers your question!
In this session, I added a few devices to the network. As I was experiencing some difficulties, I tried to send new "Permit join" requests, but the gateway ends up replying "TIMEOUTS".
When checking the serial log, the ZNP does seem quite active but I can not relate this activity to traces in the gateway log.
So apparently the gaeway is failing in this case and not the ZNP. The question is: what is causing this?
These are the logs, including the serial log, the gateway log and the applicadtion log, as well as the last CSV databae.
ZNP_SerialCom_NotReflectedToApp.zip
In reply to Ryan Brown1:
Dear Ryan
I created this new thread because it separates the issue related to the announcement of the device to the application from the fact that the gateway is non-responsive.
This thread is about the gateway not being responsive while there seems to be serial communication.
The causes for the non-responsiveness of the gateway/znp has different causes - if they appear different, I create a new thread.
Some causes have already been fixed. One of them explains why I ran into that issue when doing multiple on/off cycles of the lamps (I fixed the buffer overflow that wrote the nil byte too many), another was related to the Write Attributes Response indicating an error with one of the attributes (another memory buffer overflow), and a few others as well as unidentified ones by applying a more general fix to the zcl structures.I still have to fix the issue with the pDeviceInfo thread races (but that is not occurring here).
The fact that a device is not making its Device Announcement should not result in the gateway nor the ZNP breaking up. In fact no external condition should be breaking the gateway (except for a file corruption not due to the gateway).
The fact that 0x09ff appears as deleted concerns the other thread. I would like this one to focus on the non-responsiveness that followed. The serial log and the gateway log may help determine when it happened and hence possibly what caused it.
In reply to Mario DW:
This appears similar to pthread_mutex deadlock/race condition issue noted in the following E2E thread, can you please investigate and confirm?
Here is a relevant thread for your awareness, although I don't think it is related to the issue at hand.
I think neither of these threads are relevant to the current issue, but I am going to add the proposed protection in the first thread(the patch is already applied in the official version). The usage of the cppcheck tool is also excellent - I'll apply that as well.
I can confirm the general description of the experience with the gateway that was provided in the question.
The reason why I do not think that this is related to these other threads is my analysis below.
In summary, the ZNP is active, the Gateway is communicating towards it, but the ZNP seems to act liek a firewall: it is communicating on both sides, but nothing is going through.
So I believe that for the case described below, the issue is in the ZNP, not in the Gateway.
Analysis (logs provided further below):
The first part of the extract below is the onscreen result of a "tail" on the application log, interrupted with CTRL-C and followed with './gw' which executes "./gw_soc_fw_version_query.bin /dev/ttyO1" . I tried to reproduce the issue found with the previous GW version (mentionned in another thread). That was the starting point for a more detailed analysis of the logs.
[2020-11-10T16:31:01] attr_read_confirm_handler: Status INVALID_PARAMETER. 8:22:44] Raw=07:00:73:00:08:00:10:03:18:D7:5E 8:22:44] attr_read_confirm_handler: Received ZIGBEE_GENERIC_CNF id=01 >, n_attributelist=1, clstr=0500, attributelist=0011,0000,0000,0000,0000,0000 [2020-11-18:22:44] attr_read_confirm_handler: Status INVALID_PARAMETER. 8:22:45] REQ: addr=< type=0 ieeeaddr=00124B000760BB0A endpointid=01 >, n_attributelist=1, clstr=0500, att8:22:45] sent to GATEWAY: len=24, cmd_id=20, subsystem=19 subsystem=115 8:22:45] Raw=18:00:13:14:08:14:12:0D:08:00:11:0A:BB:60:07:00:4B:12:00:28:01:18:8:22:45] Queued command successfully; CBARG = 0 [2020-11-10T16:31:02] attr_read_confirm_handler: Received ZIGBEE_GENERIC_CNF 8:22:45] Raw=07:00:73:00:08:00:10:03:18:D8:5E root@A0F6FD520323:~# cd tools - zigbeeapp.log 1/15360 0% root@A0F6FD520323:~/tools# ./gw Using serial port: /dev/ttyO1 @115200 zbSocProcessRpc: CMD0:64, CMD1:2, not handled zbSocProcessRpc: CMD0:64, CMD1:2, not handled zbSocProcessRpc: CMD0:65, CMD1:45, not handled zbSocProcessRpc: CMD0:64, CMD1:2, not handled
After some while I interrupted this and tried to read from the "socat" virtual port that also connects to /dev/ttyO1:
root@A0F6FD520323:~/tools# ./gw_soc_fw_version_query.bin /dev/ttyV0 Using serial port: /dev/ttyV0 @115200 Received System version. Transport Protocol Version: 2 Product ID: 2 Software Release: 2.7.2 Software Revision: 20190523 root@A0F6FD520323:~/tools# date Tue Nov 10 18:37:34 UTC 2020
With the use of socat, I suspect that I can make multiple connections to the serial port as the serial log is continuously logging packs from an to the ZNP before and after this command. This means that I could inject commands to the ZNP while the gateway is running.
Also note that the application was not getting back anything before the above command and that command does not appear to impact the behavior of the gateway.
To see the commands sent by the version tool, I put a tail on the serial log in the background, and executed the readout of the version resulting in:
01 02 04 a5 00 1e 05 00 00 a5 00 00 00 1e .............. -- > 2020/11/10 18:43:24.246139 length=6 from=142988 to=142993 fe 01 64 02 02 65 ..d..e -- ./gw_soc_fw_version_query.bin /dev/ttyV0< 2020/11/10 18:43:24.824823 length=9 from=399670 to=399678 fe 04 25 45 f4 46 00 05 d3 ..%E.F... -- > 2020/11/10 18:43:24.834430 length=6 from=142994 to=142999 fe 01 65 45 c2 e3 ..eE.. -- < 2020/11/10 18:43:25.031501 length=30 from=399679 to=399708 fe 19 24 02 02 ba da be be be be be be 01 67 eb ..$...........g. 01 00 05 a6 00 1e 05 00 00 a6 00 11 00 de .............. -- > 2020/11/10 18:43:25.043552 length=6 from=143000 to=143005 fe 01 64 02 02 65 ..d..e -- root@A0F6FD520323:~/tools# ./gw_soc_fw_version_query.bin /dev/ttyV0 Using serial port: /dev/ttyV0 @115200 Received System version. Transport Protocol Version: 2 Product ID: 2 Software Release: 2.7.2 Software Revision: 20190523 root@A0F6FD520323:~/tools# < 2020/11/10 18:43:28.296007 length=1 from=399709 to=399709 ef . -- < 2020/11/10 18:43:28.298308 length=5 from=399710 to=399714 fe 00 41 02 43 ..A.C -- > 2020/11/10 18:43:28.308228 length=19 from=143006 to=143024 fe 0e 61 02 02 02 02 07 02 3b 15 34 01 01 00 00 ..a......;.4.... 00 00 70 ..p -- < 2020/11/10 18:43:31.285569 length=30 from=399715 to=399744
The frame to send the query is 'fe 00 41 02 43' and the reply is indeed the next frame.
BTW, the printf of the software revision should be inside the if(len > 5) block as software_revision is not set:
if (len > 5) { software_revision = incoming_packet[9] + (incoming_packet[10] << 8) + (incoming_packet[11] << 16) + (incoming_packet[12] << 24); } printf(" Software Revision: %u\n", software_revision); if (len <= 5) { printf(" (Revision not specified)\n"); }
The analysis of the logs from this point in time onwards show that the ZNP is still communicating, that the packets for attributes reported by an device in the network are not reported on the serial link, and that the ZNP is sending ack messages only, not any of the other commands.
[2020-11-10 18:43:24.822,814] [Z_STACK/LSTN] INFO : Receive message... [2020-11-10 18:43:24.823,281] [Z_STACK/LSTN] INFO : zstackpb zspbHandlePbCb: subsystemID:31, cmdId:15 [2020-11-10 18:43:24.823,546] [Z_STACK/LSTN] INFO : znp_misc sendNPIExpectDefaultStatusZNP: subSys:5, cmdID:45, len::4 [2020-11-10 18:43:24.823,764] [Z_STACK/LSTN] INFO : preparing to send 4 bytes, subSys 0x05, cmdId 0x45, pData: [2020-11-10 18:43:24.823,959] [Z_STACK/LSTN] INFO : [MUTEX] Lock SRSP Transaction Mutex [2020-11-10 18:43:24.826,936] [Z_STACK/LSTN] INFO : Waiting for synchronous response... [2020-11-10 18:43:24.827,291] [Z_STACK/LSTN] INFO : [MUTEX] Lock SRSP Mutex [2020-11-10 18:43:24.827,486] [Z_STACK/LSTN] INFO : [MUTEX] Wait for SRSP Cond signal... [2020-11-10 18:43:24.827,667] [Z_STACK/LSTN] INFO : [MUTEX] Unlock SRSP Mutex [2020-11-10 18:43:24.828,077] [Z_STACK/LSTN] INFO : ...sent 8 bytes to Client [2020-11-10 18:43:24.830,413] [Z_STACK/LSTN] INFO : !Done ***** The serial log corresponds to the gateway ***** sending the "4 (payload) bytes" announced above, for subsystem 0x05 (->25), ***** and command 0x45, corresponding to 8 bytes in the packet + the checksum. ***** The microsecond part of the timestamp is good as well with regards to the above. -- < 2020/11/10 18:43:24.824823 length=9 from=399670 to=399678 fe 04 25 45 f4 46 00 05 d3 ..%E.F... ***** The request to read the version is then perceived by the gateway as an incoming command. ***** I suppose that socat is responsible for that. -- > 2020/11/10 18:43:24.834430 length=6 from=142994 to=142999 fe 01 65 45 c2 e3 ..eE.. [2020-11-10 18:43:24.836,839] [Z_STACK/READ] INFO : Received 1 bytes, subSys 0x65, cmdId 0x45 [2020-11-10 18:43:24.837,239] [Z_STACK/READ] INFO : [MUTEX] SRSP Cond signal set [2020-11-10 18:43:24.837,435] [Z_STACK/READ] INFO : Client Read: (len 4): [...] -- < 2020/11/10 18:43:25.031501 length=30 from=399679 to=399708 fe 19 24 02 02 ba da be be be be be be 01 67 eb ..$...........g. 01 00 05 a6 00 1e 05 00 00 a6 00 11 00 de .............. [2020-11-10 18:43:25.027,843] [Z_STACK/LSTN] INFO : Receive message... [2020-11-10 18:43:25.028,672] [Z_STACK/LSTN] INFO : zstackpb zspbHandlePbCb: subsystemID:31, cmdId:22 [2020-11-10 18:43:25.029,531] [Z_STACK/LSTN] INFO : zstackpb Rcvd AF Data Request: addrMode: 2, dstAddr:daba, dep:1, sep:1 [2020-11-10 18:43:25.029,807] [Z_STACK/LSTN] INFO : znp_misc sendNPIExpectDefaultStatusZNP: subSys:4, cmdID:2, len::25 [2020-11-10 18:43:25.030,039] [Z_STACK/LSTN] INFO : preparing to send 25 bytes, subSys 0x04, cmdId 0x02, pData: [2020-11-10 18:43:25.030,513] [Z_STACK/LSTN] INFO : [MUTEX] Lock SRSP Transaction Mutex [2020-11-10 18:43:25.035,426] [Z_STACK/LSTN] INFO : Waiting for synchronous response... [2020-11-10 18:43:25.035,791] [Z_STACK/LSTN] INFO : [MUTEX] Lock SRSP Mutex [2020-11-10 18:43:25.035,989] [Z_STACK/LSTN] INFO : [MUTEX] Wait for SRSP Cond signal... [2020-11-10 18:43:25.036,168] [Z_STACK/LSTN] INFO : [MUTEX] Unlock SRSP Mutex ***** "25 bytes" sent by the gateway to the ZNP (+4 header, + 1 checksum). -- < 2020/11/10 18:43:25.031501 length=30 from=399679 to=399708 fe 19 24 02 02 ba da be be be be be be 01 67 eb ..$...........g. 01 00 05 a6 00 1e 05 00 00 a6 00 11 00 de .............. ***** Reception is confirmed by the [ZSTACK/READ]: > 2020/11/10 18:43:25.043552 length=6 from=143000 to=143005 fe 01 64 02 02 65 ..d..e [2020-11-10 18:43:25.051,493] [Z_STACK/READ] INFO : Received 1 bytes, subSys 0x64, cmdId 0x02 [2020-11-10 18:43:25.051,929] [Z_STACK/READ] INFO : [MUTEX] SRSP Cond signal set [2020-11-10 18:43:25.052,129] [Z_STACK/READ] INFO : Client Read: (len 4):
These traces show that the serial log is in sync with the gateway log, and that the ZNP is replying to the serial requests. Yet there are the INVALID_PARAMETER messages in the application and TIMEOUTS in the gateway log. In fact, the ZNP only sends ACK messages and some zigbee objects are sending packets to the gateway.
***** For reference this is the last record sent by the ZNP before the ones follwoing below. > 2020/11/10 18:43:33.893096 length=6 from=143037 to=143042 fe 01 65 45 c2 e3 ..eE.. -- ***** Zigbee GW log: [2020-11-10 18:43:33.894,581] [Z_STACK/READ] INFO : Received 1 bytes, subSys 0x65, cmdId 0x45 [2020-11-10 18:43:33.894,857] [Z_STACK/READ] INFO : [MUTEX] SRSP Cond signal set [2020-11-10 18:43:33.895,008] [Z_STACK/READ] INFO : Client Read: (len 4): ***** The sniffer log shows: 6186 2020-11-10 18:43:36.002655 0x46f4 â~F~R 0x0000 ZigBee HA 53 ZCL: Report Attributes, Seq: 108 6187 2020-11-10 18:43:36.003145 â~F~R IEEE 802.15.4 5 Ack ***** The device appears in the database: 00:15:8D:00:04:7B:83:69 , 0x46F4 , 0x00, 0x1037 , 1, 00:12:4B:00:10:22:82:77, 0xBE ***** But the serial log only shows communications starting at 18:43:38 ***** Reported in the Gateway log: [2020-11-10 18:43:38.513,733] [Z_STACK/LSTN] INFO : Receive message... [2020-11-10 18:43:38.514,198] [Z_STACK/LSTN] INFO : zstackpb zspbHandlePbCb: subsystemID:31, cmdId:22 [2020-11-10 18:43:38.514,577] [Z_STACK/LSTN] INFO : zstackpb Rcvd AF Data Request: addrMode: 2, dstAddr:46f4, dep:1, sep:1 [2020-11-10 18:43:38.514,817] [Z_STACK/LSTN] INFO : znp_misc sendNPIExpectDefaultStatusZNP: subSys:4, cmdID:2, len::25 [2020-11-10 18:43:38.515,046] [Z_STACK/LSTN] INFO : preparing to send 25 bytes, subSys 0x04, cmdId 0x02, pData: ***** 25 bytes sent: < 2020/11/10 18:43:38.516144 length=30 from=399784 to=399813 fe 19 24 02 02 f4 46 be be be be be be 01 67 eb ..$...F.......g. 01 02 04 a9 00 1e 05 00 00 a9 00 00 00 1e .............. -- [2020-11-10 18:43:38.515,244] [Z_STACK/LSTN] INFO : [MUTEX] Lock SRSP Transaction Mutex [2020-11-10 18:43:38.523,622] [Z_STACK/LSTN] INFO : Waiting for synchronous response... [2020-11-10 18:43:38.523,993] [Z_STACK/LSTN] INFO : [MUTEX] Lock SRSP Mutex [2020-11-10 18:43:38.524,191] [Z_STACK/LSTN] INFO : [MUTEX] Wait for SRSP Cond signal... [2020-11-10 18:43:38.524,370] [Z_STACK/LSTN] INFO : [MUTEX] Unlock SRSP Mutex [2020-11-10 18:43:38.524,795] [Z_STACK/LSTN] INFO : ...sent 8 bytes to Client [2020-11-10 18:43:38.525,079] [Z_STACK/LSTN] INFO : !Done > 2020/11/10 18:43:38.534702 length=6 from=143043 to=143048 fe 01 64 02 02 65 ..d..e -- [2020-11-10 18:43:38.537,441] [Z_STACK/READ] INFO : Received 1 bytes, subSys 0x64, cmdId 0x02 [2020-11-10 18:43:38.537,877] [Z_STACK/READ] INFO : [MUTEX] SRSP Cond signal set [2020-11-10 18:43:38.538,080] [Z_STACK/READ] INFO : Client Read: (len 4): [2020-11-10 18:43:39.185,593] [Z_STACK/LSTN] INFO : Receive message... [2020-11-10 18:43:39.186,019] [Z_STACK/LSTN] INFO : zstackpb zspbHandlePbCb: subsystemID:31, cmdId:22 [2020-11-10 18:43:39.186,216] [Z_STACK/LSTN] INFO : zstackpb Rcvd AF Data Request: addrMode: 2, dstAddr:daba, dep:1, sep:1 [2020-11-10 18:43:39.186,343] [Z_STACK/LSTN] INFO : znp_misc sendNPIExpectDefaultStatusZNP: subSys:4, cmdID:2, len::25 [2020-11-10 18:43:39.186,456] [Z_STACK/LSTN] INFO : preparing to send 25 bytes, subSys 0x04, cmdId 0x02, pData: < 2020/11/10 18:43:39.187148 length=30 from=399814 to=399843 fe 19 24 02 02 ba da be be be be be be 01 67 eb ..$...........g. 01 00 05 aa 00 1e 05 00 00 aa 00 11 00 de .............. -- > 2020/11/10 18:43:39.198683 length=6 from=143049 to=143054 fe 01 64 02 02 65 ..d..e -- [2020-11-10 18:43:38.537,441] [Z_STACK/READ] INFO : Received 1 bytes, subSys 0x64, cmdId 0x02 [2020-11-10 18:43:38.537,877] [Z_STACK/READ] INFO : [MUTEX] SRSP Cond signal set [2020-11-10 18:43:38.538,080] [Z_STACK/READ] INFO : Client Read: (len 4):
So at least in this case, the issue does not seem to be with the gateway itself that seems to be a lot more stable (no more memory issues), but the issue is with the ZNP. The ZNP stoppped relaying the requests on its serial interface to the Zigbee RF sie, while still replying to these serial requests. And the same time the ZNP acknowledges Zigbee packets but not communicate them on the serial interface.
What could be causing that? How to fix it? Or how to get more information to determine the cause?
Logs:ZNP_PartiallyResponsive.zip
Outcome of the 'cppcheck' applied to gateway code:
[ipclib/server/npi_lnx_ipc.c:1921]: (error) Memory leak: errorStr char *errorStr = (char *)malloc(30); Easy fix: char errorStr[30]; [ipclib/server/npi_lnx_ipc.c:2549]: (error) Memory leak: strBuf Obvious one: strBuf = (char*) malloc(128); // line deleted. strBuf = pStrBufRoot; [ipclib/server/npi_lnx_ipc.c:410]: (error) Undefined behavior: Variable 'fullStr' is used as parameter and destination in s[n]printf(). Meant to append to the string... sprintf(fullStr, "%s] %s", fullStr, inStr); -> sprintf(fullStr+strlen(fullStr), "] %s", inStr); [ipclib/server/npi_lnx_ipc.c:413]: (error) Undefined behavior: Variable 'fullStr' is used as parameter and destination in s[n]printf(). Another append that could be merged with the append above: sprintf(fullStr, "%s. Error: %.8X\n", fullStr, npi_ipc_errno); -> sprintf(fullStr+strlen(fullStr), ". Error: %.8X\n", npi_ipc_errno); Checking ../srvwrapper/api_server.c... [../srvwrapper/api_server.c:524]: (error) Memory leak: errorStr [../srvwrapper/api_server.c:992]: (error) Undefined behavior: Variable 'fullStr' is used as parameter and destination in s[n]printf(). [../srvwrapper/api_server.c:995]: (error) Undefined behavior: Variable 'fullStr' is used as parameter and destination in s[n]printf(). Checking ../sdb/SimpleDBTxt.c... Could happen if (record[0] != SDBT_PENDING_COMMENT_FORMAT_CHARACTER) [../sdb/SimpleDBTxt.c:150]: (error) Uninitialized variable: rc -> Initialised to FALSE. Checking ../srvepconfig/serverep.c... False positive: [../srvepconfig/serverep.c:2172]: (error) Memory leak: pNewAttrList Complex, but seems false positive. [../srvepconfig/serverep.c:2185]: (error) Memory leak: pNewAttrList Checking ../../../../Components/stack/zcl/zcl.c... Could be undefined when i=0, initialise to 0 [../../../../Components/stack/zcl/zcl.c:4834]: (error) Uninitialized variable: j Checking ../../../../Components/stack/zcl/zcl_green_power.c... Not set unless error -> initialise as ZSuccess [../../../../Components/stack/zcl/zcl_green_power.c:389]: (error) Uninitialized variable: status Checking ../serverpb/gatewayp2p.c... -> Initialise to FALSE, could be undefined depending on pRsp [../serverpb/gatewayp2p.c:161]: (error) Uninitialized variable: isSuccess Checking aps_groups.c... -> Initialise to ZSTATUS_VALUES__ZFailure [aps_groups.c:149]: (error) Uninitialized variable: status -> Initialise to FALSE [aps_groups.c:328]: (error) Uninitialized variable: status Checking gatewayservices.c... -> Free the record. [gatewayservices.c:805]: (error) Memory leak: pNewAttrListRecord -> Initialise to 0 [gatewayservices.c:1116]: (error) Uninitialized variable: clusterMatchCount Checking gatewaysrvr.c... -> Free the record [gatewaysrvr.c:7146]: (error) Memory leak: pCfgReportCmd Checking zcl_port.c... -> Init as afStatus_FAILED [zcl_port.c:507]: (error) Uninitialized variable: status Checking OtaServer.c... -> move fopen after malloc. [OtaServer.c:327]: (error) Resource leak: pfile -> move fopen after malloc. [OtaServer.c:524]: (error) Resource leak: pfile Checking zcl_port.c... -> Init as afStatus_FAILED [zcl_port.c:326]: (error) Uninitialized variable: status
Thank you for that detailed analysis, if the issue involves the ZNP malfunctioning then as with the other threads it will require further debugging of the CC2530 to determine the MCU state.
with my new tool, it is now easier to interpret the serial log, we we can see the "version" request and response:
[2020-11-10 18:43:24.824823] < [ZDO/SREQ] **EXT_ROUTE_DISC** (SYS:5/TYPE:20/CMD:45) ( 9)::fe 04 25 45 f4 46 00 05 d3 [2020-11-10 18:43:24.834430] > [ZDO/SRSP] **EXT_ROUTE_DISC** (SYS:5/TYPE:60/CMD:45) ( 6)::fe 01 65 45 c2 e3 [2020-11-10 18:43:25.031501] < [AF/SREQ] **DATA_REQUEST_EXT** (SYS:4/TYPE:20/CMD:02) ( 30)::fe 19 24 02 02 ba da be be be be be be 01 67 eb 01 00 05 a6 00 1e 05 00 00 a6 00 11 00 de [2020-11-10 18:43:25.043552] > [AF/SRSP] **DATA_REQUEST_EXT** (SYS:4/TYPE:60/CMD:02) ( 6)::fe 01 64 02 02 65 [2020-11-10 18:43:28.296007] < ( 1)::ef [2020-11-10 18:43:28.298308] < [SYS/AREQ] **VERSION** (SYS:1/TYPE:40/CMD:02) ( 5)::fe 00 41 02 43 [2020-11-10 18:43:28.308228] > [SYS/SRSP] **VERSION** (SYS:1/TYPE:60/CMD:02) ( 19)::fe 0e 61 02 02 02 02 07 02 3b 15 34 01 01 00 00 00 00 70 [2020-11-10 18:43:31.285569] < [AF/SREQ] **DATA_REQUEST_EXT** (SYS:4/TYPE:20/CMD:02) ( 30)::fe 19 24 02 02 f4 46 be be be be be be 01 67 eb 01 02 04 a7 00 1e 05 00 00 a7 00 00 00 1e [2020-11-10 18:43:31.295828] > [AF/SRSP] **DATA_REQUEST_EXT** (SYS:4/TYPE:60/CMD:02) ( 6)::fe 01 64 02 02 65 [2020-11-10 18:43:32.325084] < [AF/SREQ] **DATA_REQUEST_EXT** (SYS:4/TYPE:20/CMD:02) ( 30)::fe 19 24 02 02 ba da be be be be be be 01 67 eb 01 00 05 a8 00 1e 05 00 00 a8 00 11 00 de [2020-11-10 18:43:32.342772] > [AF/SRSP] **DATA_REQUEST_EXT** (SYS:4/TYPE:60/CMD:02) ( 6)::fe 01 64 02 02 65 [2020-11-10 18:43:33.884446] < [ZDO/SREQ] **EXT_ROUTE_DISC** (SYS:5/TYPE:20/CMD:45) ( 9)::fe 04 25 45 ba da 00 05 01 [2020-11-10 18:43:33.893096] > [ZDO/SRSP] **EXT_ROUTE_DISC** (SYS:5/TYPE:60/CMD:45) ( 6)::fe 01 65 45 c2 e3
I do not know if these "DATA_REQUEST_EXT" requests are a sign of the ZNP dysfunctionning, but the ZNP is replying (">") to requests from the gateway ("<").
Earlier in the serial log we rather have this kind of communication:
[2020-11-09 18:02:31.049356] > [AF/AREQ] **INCOMING_MSG** (SYS:4/TYPE:40/CMD:81) ( 34)::fe 1d 44 81 00 00 00 05 dc 9e 01 01 00 5c 00 c6 77 6c 00 00 09 19 3a 00 20 00 00 ff 00 00 dc 9e 1d b4 [2020-11-09 18:02:32.470648] > [AF/AREQ] **INCOMING_MSG** (SYS:4/TYPE:40/CMD:81) ( 32)::fe 1b 44 81 00 00 00 05 dc 9e 01 01 00 54 00 1f 89 6c 00 00 07 19 3b 01 0d 00 63 11 dc 9e 1d 33 [2020-11-09 18:02:32.516165] < [AF/SREQ] **DATA_REQUEST_EXT** (SYS:4/TYPE:20/CMD:02) ( 30)::fe 19 24 02 02 00 00 be be be be be be ff 00 00 01 00 05 62 00 1e 05 00 11 39 00 00 60 f7 [2020-11-09 18:02:32.530071] > [AF/SRSP] **DATA_REQUEST_EXT** (SYS:4/TYPE:60/CMD:02) ( 6)::fe 01 64 02 00 67 [2020-11-09 18:02:32.536348] > [AF/AREQ] **DATA_CONFIRM** (SYS:4/TYPE:40/CMD:80) ( 38)::fe 03 44 80 00 01 62 a4 fe 19 44 81 00 00 00 05 00 00 01 0e 00 ff 00 00 00 00 00 00 05 11 39 00 00 60 00 00 00 64 [2020-11-09 18:02:32.544601] > [AF/AREQ] **INCOMING_MSG** (SYS:4/TYPE:40/CMD:81) ( 30)::fe 19 44 81 00 00 00 05 00 00 01 01 00 ff 00 00 00 00 00 00 05 11 39 00 00 60 00 00 00 6b [2020-11-09 18:02:34.469630] > [AF/AREQ] **INCOMING_MSG** (SYS:4/TYPE:40/CMD:81) ( 32)::fe 1b 44 81 00 00 00 05 dc 9e 01 01 00 41 00 86 a1 6c 00 00 07 19 3c 01 0d 00 63 11 dc 9e 1d 90 [2020-11-09 18:02:34.514916] < [AF/SREQ] **DATA_REQUEST_EXT** (SYS:4/TYPE:20/CMD:02) ( 30)::fe 19 24 02 02 00 00 be be be be be be ff 00 00 01 00 05 63 00 1e 05 00 11 39 00 00 61 f7 [2020-11-09 18:02:34.532448] > [AF/SRSP] **DATA_REQUEST_EXT** (SYS:4/TYPE:60/CMD:02) ( 14)::fe 01 64 02 00 67 fe 03 44 80 00 01 63 a5 [2020-11-09 18:02:34.537728] > [AF/AREQ] **INCOMING_MSG** (SYS:4/TYPE:40/CMD:81) ( 60)::fe 19 44 81 00 00 00 05 00 00 01 0e 00 ff 00 00 00 00 00 00 05 11 39 00 00 61 00 00 00 65 fe 19 44 81 00 00 00 05 00 00 01 01 00 ff 00 00 00 00 00 00 05 11 39 00 00 61 00 00 00 6a [2020-11-09 18:02:36.480387] > [AF/AREQ] **INCOMING_MSG** (SYS:4/TYPE:40/CMD:81) ( 32)::fe 1b 44 81 00 00 00 05 dc 9e 01 01 00 46 00 0f ba 6c 00 00 07 19 3d 01 0d 00 63 11 dc 9e 1d 04 [2020-11-09 18:02:36.564743] < [AF/SREQ] **DATA_REQUEST_EXT** (SYS:4/TYPE:20/CMD:02) ( 30)::fe 19 24 02 02 00 00 be be be be be be ff 00 00 01 00 05 64 00 1e 05 00 11 39 00 00 62 f3 [2020-11-09 18:02:36.580941] > [AF/SRSP] **DATA_REQUEST_EXT** (SYS:4/TYPE:60/CMD:02) ( 6)::fe 01 64 02 00 67 [2020-11-09 18:02:36.587918] > [AF/AREQ] **DATA_CONFIRM** (SYS:4/TYPE:40/CMD:80) ( 38)::fe 03 44 80 00 01 64 a2 fe 19 44 81 00 00 00 05 00 00 01 0e 00 ff 00 00 00 00 00 00 05 11 39 00 00 62 00 00 00 66 [2020-11-09 18:02:36.614779] > [AF/AREQ] **INCOMING_MSG** (SYS:4/TYPE:40/CMD:81) ( 30)::fe 19 44 81 00 00 00 05 00 00 01 01 00 ff 00 00 00 00 00 00 05 11 39 00 00 62 00 00 00 69 [2020-11-09 18:07:38.882274] > [AF/AREQ] **INCOMING_MSG** (SYS:4/TYPE:40/CMD:81) ( 32)::fe 1b 44 81 00 00 01 00 dc 9e 01 01 00 44 00 73 25 7b 00 00 07 18 3e 0a 21 00 20 c8 dc 9e 1d 49
So a fair amount of "INCOMING_MSG" with "DATA_REQUEST_EXT" and "DATA_CONFIRM" exchanges as well.
The last incoming message before [2020-11-10 18:43:24.824823] is:
[2020-11-10 00:32:58.761572] > [AF/AREQ] **INCOMING_MSG** (SYS:4/TYPE:40/CMD:81) ( 32)::fe 1b 44 81 00 00 01 00 dc 9e 01 01 00 5e 00 27 93 cd 00 00 07 18 37 0a 21 00 20 c8 dc 9e 1d 0e
What do you conclude of this?seriallog.log.15.zip
Hey le_top,
Monitor and Test API packets are formatted as such:
SOF | LEN | CMD0 | CMD1 | DATA | FCS
Where SOF is 0xFE and LEN contains the number of DATA bits. In all of the DATA_REQUEST_EXT ZNP responses it can be observed that DATA is 0x02 which is the INVALID_PARAMETER status. There can be multiple causes of this in Z-Stack. The EXT_ROUTE_DISC response with DATA of 0xC2 which is a ZNwkInvalidRequest.
Hi Ryan
I'll extend my MT packet decoder because my end goal is to fix what is causing this and other unexpected behaviors.
I guess that the next step is that I examine and debug the ZNP?!
Kind regards
Mario