This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 25
Part Number: CC2652P
Hi,
I am planning to build a ZigBee 3.0 based coordinator which act as a centralized trust center.
I also would like to change the security key dynamically. That means trust center should be able to tell other devices to move to new key and start communicating with this key.
Does TI support this feature now?
If yes can you explain how can i achieve that?
Thanks,
Vikas
Yes, TI Z-Stack supports this Zigbee 3.0 feature by default.
If my post answers your question, please click on "This Resolved my issue" button to benefit others who have the same issue.
YK Chen
Build OpenThread Sleepy End Device doorlock prototype to test with Rasperry Pi OpenThread Border Router
How to use two UARTs in CC26x2 and CC13x2
SwitchBot DIY using LPSTK-CC1352R , SG90 servo motor, and ProjectZero to away from COVID-19.
How to use two endpoints in SIMPLELINK-CC13X2-26X2-SDK Z-Stack.
CC13xx TRX WOR project.
How to create a periodic event to toggle BLE Advertising in CC26xx simple_peripheral example
How to use indication in simple_peripheral example and use Btool to enable indication
How to check APS ack in TI Z-Stack
How to detect button hold in CC26x2, CC13x0, CC13x2 SDK.
660 Zigbee devices in the same Zigbee network!
Hi Vikas,
This feature is covered in part 3 of the Zigbee Security SLA.
Regards,Ryan
To better aid the community, please click on the "This Resolved my issue" button whenever a post answers your question!