Hi,All,
Currently, RF engineers test the receiving sensitivity of CC2531 through RF instruments:
CC2531 is in packetRx state in SmartRf Studio,
The RF instrument sends ten 127-byte data packets quickly (about 5ms), and SmartRf Studio shows that 2531 can only receive 1-2 packets;
The RF instrument quickly sends 1000 127-byte data packets, and SmartRf Studio shows that CC2531 can only receive dozens of packets;
In addition, in SmartRf Studio, CC2531 is basically normal as the receiving/transmitting terminal, and the fastest sending interval is about 30-40ms;
For the scene of rapid data sending by the instrument, how to improve the statistics of CC2531 data reception in SmartRf Studio?